DÜRR

Rittal Reference Project – Industrial Enclosures

 
Give way for TS 8
The project

Whether in the sign of the star, the rings, or Wolfsburg, the coachbuilder carman builds the requested vehicles. This implies highest flexibility that was also required when realising the new finishing coat line.
Give way for TS 8

TS 8    Optimum cooperation

The supplier of the painting plant, » DÜRR-System GmbH, has instructed the Neunburg company F.EE to realise the control from concept finding via project planning to installation. The complete project could be realised within eight weeks. After further six weeks the finishing coat line commenced operation.


Everything with system

The » Rittal Top Enclosure System TS 8 was perfectly suitable for the control of the state-of-the-art finishing line where all three currently produced body shell types. In five stations approximately 30 metres of enclosures are bayed. 14 climate control doors dissipate the heat from the enclosures. In addition many components from the comprehensive Rittal range are used.

© 2012, Rittal
Imprint | Legals
Rittal - Switch to perfection