Industrial Enclosures

Rittal reference projects

 
TS 8 special models in Singapore

Thanks to the fusion of seven islands in Singapore an impressive economic centre is arising. Rittal supplied more than 400 TS 8 enclosures in various variants for Shell Chemicals» Shell Chemicals and Singapore Power. » more
 
     Back-to-back baying with TS 8

With the TS 8 enclosure Natus found the solution for space and transport problems. Thanks to back-to-back baying installation of enclosures could be made from both sides and it was possible to transport the enclosures individually in a height of up to 25 m. » more
 
Safe is safe with TS 8

Free-standing and unprotected extinguisher bottles in the production area and the freely accessible control centre is a problem for many plant operators. The danger is too high that the fire protection system is damaged by environmental influences like dust or humidity and therefore fails in case of emergency. » more
 
     Give way for TS 8

Whether in the sign of the star, the rings, or Wolfsburg, the coachbuilder carman builds the requested vehicles. This implies highest flexibility that was also required when realising the new finishing coat line. » more

© 2012, Rittal
Imprint | Legals
Rittal - Umschalten auf Perfektion