Natus

Rittal Reference Project – Industrial Enclosures

 
Back-to-back baying with the TS 8
Back-to-back baying with the TS 8
The project

Intermoselle is a Dyckerhoff subsidiary that produces clinker for concrete production in Rumelange, Luxemburg. After approx. thirty years the complete control system of the plant which is decentrally accommodated in five switch rooms will be modernised.

Flexible solutions with Rittal TS 8 Flexible solutions with Rittal TS 8

» Natus GmbH & Co. KG based in Trier, commissioned to realise the new control system were confronted with difficult ambient conditions. With the » TS 8 Natus found the solution for space and transport problems. Thanks to the back-to-back baying it was possible to install the enclosures from both sides and to transport them individually in a height of up to 25 m.


Smooth run despite time pressure

Smooth run despite time pressure
The control enclosures are installed and finally accepted on site at Natus. In the first four weeks of January during several conversion stages, the control is mounted on site and commissioned. No problem for Natus because Rittal is a reliable and flexible partner.


© 2012, Rittal
Imprint | Legals
Rittal - Umschalten auf Perfektion