What does UL mean? UL or Underwriter Laboratory was founded in 1894 as a non-profit-making organisation for testing and certification. UL operates five testing laboratories in the United States and subsidiaries worldwide, with an emphasis on product testing aimed at general safety.
- International regulations and standards such as NEMA and IEC are used as a basis by manufacturers for product development and subsequent testing.
- Nationally recognised testing laboratories confirm and certify that a product meets specific standards.
- In North America, this is carried out by organisations such as UL or CSA (Canadian Standard Association).
For many applications, only UL and/or CSA-approved products are acceptable. It is therefore advisable to ensure that electrical control systems intended for use in North America are designed with UL-approved components.
UL product labelling: What does “UL listed“ or “UL recognized“ mean?
When labelling UL-approved products, a general distinction is made between Recognized Components and Listed Components:
Recognized Components This label is used on products that are not complete in terms of their application.
- These products are listed in the UL’s “yellow component database”.
- The correct use of such components must make due allowance for the “Conditions of Acceptability”, listing the framework conditions and application parameters approved by the UL.
- These may be deratings, application/use specifications in conjunction with additional active/passive components, as for example specific fuse types.
- Furthermore, the application field of “branch circuits“ or “feeder circuits“ of the component is determined by the COAs.
Listed Components This symbol is used in products that offer a complete function in themselves. Without consideration of the COAs.
- These products are listed in the UL’s “green component database”.
They may be used without restriction in accordance with the tested rating. For this all technical data must be visible on the type plate. Separate assembly instructions must be directly attached to the device or allocated to the product on a package insert. » Important benefits and added value with RiLine60
What is the difference between UL 508 und UL 508A in application? UL 508 describes the standard for Industrial Control Equipment like Rittal busbar systems, SV components, switchgear etc. In addition the UL 508 is divided in sections A,B,C ... to classify the application field of the tested devices:
- A - Magnetic, manual and solid starters
- B - Thermal, magnetic, and solid overload relays
- C - Push buttons, selector switches and pilot lights
- D - Control circuit switches and relays
UL 508A is the standard for the assembly of switchgear for Industrial Control Panels that must be observed by the plant engineers. UL 508A combines all necessary UL standards including UL 508 which are necessary for switchgear construction. For example, this standard contains information on:
- Machine controllers
- Elevator controllers
- Crane controllers
- Equipment for heating, air-conditioning and ventilation systems
Both standards describe control systems for general industrial applications with a rated voltage of up to 600 V. The maximum permissible ambient temperature is 40°C.
How does the US acceptance procedure for electrical plants work? Every piece of electrical equipment (machine/plant) is tested by the competent local inspector (AHJ = Authority Having Jurisdiction) prior to commissioning. The AHJ has the final say with regard to commissioning.
- All AHJs use Standard NFPA 70 (NFPA = National Fire Protection Association) as a basis, which is generally regarded as the NEC (National Electrical Code).
- The AHJ considers the use of UL-recognized or UL-listed components an important indication that a system complies with the safety requirements to NFPA 70.
- This saves time and money during construction and commissioning of the equipment, as the UL symbol indicates that testing of the components and/or of the system did not reveal any foreseeable risks with regard to fire, electric shock and associated dangers.
For appliances with recognized labelling, the UL inspector inspects the COAs he can see in the UL-file.
Glossary of commonly used UL directives for low-voltage distributors (switch-/controlgears)
- UL 248 Low-Voltage Fuses
- UL 486 Equipment Wiring Terminals for use with Aluminium and/or Copper Conductors
- UL 489 Molded-Case Circuit breakers, Molded-Case Switch and Circuit-Breaker Enclosures
- UL 508 Industrial Control Equipment
- UL 508A Industrial Control Panels
- UL 512 Fuseholders
- UL 845 Motor Control Centers (MCC`s)
- UL 891 Switchboards
|