Energy Efficiency in Cooling Systems

Challenge and responsibility. We're ready.


It's important to talk about energy efficiency.
And it's our job to put the resulting ideas into practice.

Energy efficiency is a key topic of the future for industrial production processes and IT infrastructures. In view of increasing problems with the global climate and the environment, coupled with rising energy prices, it is essential that existing resources are used more efficiently. As a leading manufacturer of enclosure system, server rack and Data Centre climate technology, we are not just preparing to face the challenges and responsibilities of the future. Our investments in recent years have, without a doubt, led to above-average energy efficiency. The chief focus of our development goals is to improve the overall efficiency of our products. This is important because discerning customers make investment decisions based on the principle of TBU (Total Benefit of Usership).

Our cooling systems undergo additional neutral assessments by external experts to check both their energy efficiency and overall efficiency. To this end, we work closely with independent test institutes.


The three area markings:

» Reduced energy consumption through a higher level of efficiency.

» Reduced consumption of filter media through the use of waste-reducing nanotechnology.

» Sustained high level of efficiency in contaminated ambient air through the use of nanotechnology.



Rittal fulfils three energy efficiency requirements.
Technology you can rely on.

The new efficiency label from Rittal in accordance with DIN EN ISO 14021 identifies all cooling systems that make a significant contribution to environmental protection. These cooling systems far exceed the requirements of DIN 3168.

Energy efficiency at Rittal covers several dimensions. That's why we have augmented our efficiency label with three area markings:
Energy, Waste and Performance.
 
Further information
 
Disclaimer
The values stated here serve for estimating potential savings of the enclosure cooling units in a defined customer environment.
The values determined in the calculation do not necessarily comply with actual obtained values in customer environments. For this reason all data given are without obligation.
 
 
   
   

© 2010, Rittal
Imprint | Legals
Rittal - Umschalten auf Perfektion