Rittal cooling technology - wind power plants in Egypt
On the road to success with teamwork
The power plant experts from » Nordex GmbH enjoy an excellent reputation worldwide where innovative technology in the field of alternative wind power is required. Strong winds, fine, saline sand and massive temperature fluctuations exceptionally affect the sensitive control components.
In close collaboration with Rittal an overall concept has been developed that helps to solve problems in advance.
Convincing in case of climate fluctuations
After comprehensive laboratory tests the combination of roof-mounted cooling units with enclosure internal fans was chosen. An integral heater avoids the formation of condensate at desert-like temperature fluctuations and helps to prevent damage from humidity caused by condensation.
Enclosure internal fan: Targeted cooling, where it is needed
Ideal air throughput, even under extreme conditions: the strong roof-mounted cooling units from Rittal.
"Pro Ozone" is the keyword!
For a long time Rittal has been involved in active environment protection. Especially in the field of enclosure climate control, environment-friendly coolants are used.
Materials are used that offer maximum cooling results at minimum environment pollution. A small step with regard to the global frame, however a step that is worthwhile. The climate on our earth reacts extremely sensitively to negative human interventions. We are now being called upon!