Solution visualisations

 






3D visualisation and 3D animation service product visualisation – a picture is worth more than a 1000 words

" Imagine..." that the source of error of personal interpretation is omitted thanks to 3D visualisation. Pictures are the optimum basis for non-verbal communication as expressed in the saying "a picture is worth more than a 1000 words". Due to the digital output format that can be distributed via the WWW, partners can be supplied globally with an identical level of knowledge. Animated films help to design, with easy access, subjects that are difficult to explain or unable to be presented in reality. For example, concealed elements can be visualised by means of transparent views. Indirect apparent product potential can thus come to the fore and be focussed on.

How is this created in our company? - very easily!
By means of a visualisation software virtual 3-dimensional computer models are generated and rendered. The use of light, shadow and surface structure results in the creation of scenes that seem to be real and can be moved when animated. Working in virtual space offers the opportunity to visualise virtual ideas that do not exist but also to include existing 3D models in application scenes. Thus an already existing plant, machine or environment can be photographed and filled with virtual models.

With the appropriate data we are able to display your Rittal solution in an early stage in the application area or equipped with your specific application. This can be more informative than the creation of a prototype.

Flexible in shape and colour
One of the benefits of this technology is the realistic display of combinations or variants of products and colours. Changes in design - whether in technical or visual - can be realised quickly.

For more information about this innovative Rittal Service, contact your Rittal specialist.

« back
   
More information
 
 
   
   

© 2010, Rittal
Imprint | Legals
 
Rittal - Switch to perfection