RiDiag
Diagnosis of the operating behaviour of cooling units

The advantage to you:
On connection to a PC the following data can be retrieved:
- Error messages issued and their frequency and time of issue
- Maximum environmental temperature recorded
- Minimal internal enclosure temperature recorded
- Duty cycle and utilisation of the cooling unit
To connect a microcontroller-regulated Rittal cooling unit to the serial port in your PC, you require a special cable, which you can obtain from Rittal using the order Model No. SZ 3159.000.
- With RiDiag, diagnosis of the operating behaviour of microcontroller-regulated cooling units is possible.
Every diagnosis check can be saved as a file and therefore used as documentation of the operating behaviour. All setup parameters, such as the internal enclosure temperature, sensitivity of the filter mat monitoring etc. can be modified and saved using RiDiag.

-
- If you have any technical questions, please contact the following contact person.