Press releases

Image source: Rittal

Hannover Messe 2017: Rittal demonstrates all-round expertise for industry and IT solutions

2017-03-29. Its presentation at Hannover Messe is highly practical, with a strong focus on solutions. The system supplier is addressing the current challenges facing plant engineers/operators and IT decision-makers under the motto “Our Expertise. Your Benefit.”

Read article!
  • Rittal and IBM expand alliance for professional data centres

    2016-09-23. Rittal and IBM have expanded their existing relationship globally. The collaboration, which had previously only covered the EMEA region, has now been extended to a worldwide one thanks to the positive experience gained in recent months.

  • Safety first – the highest possible IT protection

    2016-09-06. From 18 to 20 October 2016, Rittal will be exhibiting the latest information technology infrastructure solutions at the “it-sa” IT security trade show in Nuremberg. The products presented will range from single IT racks to modular systems for turnkey data centres.

  • How enterprises can tighten up their IT security

    2016-08-29. The baseline protection guidelines issued by the German Federal Office for Information Security (BSI) are a veritable goldmine of pointers to circumstances with the potential to jeopardise IT operations. The BSI catalogues define five categories ranging from basic threats to deliberate acts.

  • Installing cables easily

    2016-08-23. If cables can be easily installed in the enclosure in an EMC-compatible way, and if strain relief can be provided at the same time, this will save an enormous amount of time during electrical installation work. This is particularly true if it can be achieved with a single component such as the Rittal cable clamp rail

  • Rittal lays foundation stone for new, highly advanced production plant

    2016-08-19. Rittal plans to build the world’s most advanced production plant for compact enclosures in the German State of Hesse. The company also intends to upgrade factories in nearby Rittershausen and Hof. The projects will prepare Rittal, a world-leading provider of industrial enclosure systems, for future challenges.

  • A cool climate for IT environments – even at the height of summer

    2016-08-17. The right climate control system is essential for any high-availability IT environment. Without effective cooling, the systems would overheat in a few moments. Consider a similar scenario – a car engine. If the water pump fails, the circulation of coolant is disrupted – frying, and potentially destroying, the engine.

  • Safe working on enclosures

    2016-08-10. When connecting electrical devices to switchgear, safety of man and machine must be taken into account. Thus, circuits with a rated current of ≤ 20 A which supply sockets in or on enclosures of machines must be fused by means of a residual-current protective device (rated differential current of ≤ 30mA).

  • Rittal and EPLAN at WindEnergy 2016 in Hamburg

    2016-08-03. Cutting electricity production costs is a constant challenge for the wind energy sector. To stay competitive, wind turbine manufacturers must invest in new plant technology that combines cost and energy efficiency.