Nov 8, 2022

New Rittal RiMatrix Micro Data Centers

An efficiency bundle for even greater speed

They are compact, powerful, and fully-fledged homes for IT hardware. Rittal RiMatrix Micro Data Centers, with such matching OT components as rack, power, cooling, monitoring and security, ensure that the IT is securely packaged and operates with the smallest carbon emissions, regardless of the location. Moreover, the combination of global standardisation and adaptability means that these new packages make even better use of their advantages.

Digital transformation is reaching more areas in everyday life and industry. This is also changing the demands on the IT infrastructure. Rapidly growing data volumes must be processed directly on site far more frequently, whether for reasons of latency in edge computing in the factory or to send fewer data to the cloud. The goal is to increase data sovereignty and cut latency times. Therefore, IT infrastructures must be fast to implement, as well as powerful, highly available, well-protected and energy-efficient.

High protection levels in a confined space
This is ensured by the RiMatrix Micro Data Center, a compact home for fully fledged data centres with every key OT system elements such as matching rack, power, cooling, monitoring and security features. Besides being used as an edge data centre in harsh environments, it can also provide the complete IT infrastructure for administrations and supermarkets without extensive structural changes, for example. The RiMatrix Micro Data Center can also back up data at locations calling for a high level of physical protection.

Standardised, adaptable and climate-friendly
The new Rittal Micro Data Centers are pre-configured for different output classes and applications, with feasibility checks for customised applications. They are available worldwide and fast. This saves time, speeds up configuration and cuts energy consumption, as the components in the overall system are coordinated.
Rittal has also developed a configurator that allows sales partners to select the right data centres for their clients. This online tool offers a feasibility check, ensures an error-free ordering procedure, and slashes the time needed for selection, delivery and commissioning.