LLDP-EXT-MED-MIB DEFINITIONS ::= BEGIN

IMPORTS
    MODULE-IDENTITY, OBJECT-TYPE, Integer32, Gauge32, Unsigned32, 
    NOTIFICATION-TYPE
        FROM SNMPv2-SMI
    TEXTUAL-CONVENTION, TruthValue
        FROM SNMPv2-TC
    MODULE-COMPLIANCE, OBJECT-GROUP, NOTIFICATION-GROUP
        FROM SNMPv2-CONF
    lldpExtensions, lldpLocPortNum, 
    lldpRemTimeMark, lldpRemLocalPortNum, lldpRemIndex,
    lldpPortConfigEntry, lldpRemChassisIdSubtype, lldpRemChassisId
        FROM LLDP-MIB
    Dscp
        FROM DIFFSERV-DSCP-TC
    SnmpAdminString
        FROM SNMP-FRAMEWORK-MIB;

lldpXMedMIB MODULE-IDENTITY
    LAST-UPDATED "200507280000Z" -- July 28th, 2005
    ORGANIZATION "TIA TR41.4 Working Group"
    CONTACT-INFO 
"  WG-URL: http://www.tiaonline.org/standards/sfg/scope.cfm#TR-41.4
             WG-EMail: tr41@tiacomm.org
              Contact: Chair, TIA TR-41
               Postal: Telecommunications Industry Association
                       2500 Wilson Blvd., Suite 300
                       Arlington, VA 22201 USA
                  Tel: (703) 907-7700
               E-mail: tr41@tiacomm.org"
    DESCRIPTION
            "The LLDP Management Information Base extension module for
            TIA-TR41.4 media endpoint discovery information.

            In order to assure the uniqueness of the LLDP-MIB,
            lldpXMedMIB is branched from lldpExtensions using the TIA OUI 
            value as the node.  An OUI/'company_id' is a 24 bit globally 
            unique assigned number referenced by various standards.

            Copyright (C) TIA (2005).  This version of this MIB module
            is published as Section 13.3 of ANSI/TIA-1057.

            See the standard itself for full legal notices."
    REVISION        "200507280000Z" -- July 28th, 2005
    DESCRIPTION
            "Published as part of ANSI/TIA-1057."
   ::= { lldpExtensions 4795 } 

------------------------------------------------------------------------------
------------------------------------------------------------------------------
--
-- LLDP-MED Information
--
------------------------------------------------------------------------------
------------------------------------------------------------------------------

lldpXMedNotifications    OBJECT IDENTIFIER ::= { lldpXMedMIB 0 }
lldpXMedObjects          OBJECT IDENTIFIER ::= { lldpXMedMIB 1 }

-- LLDP MED Extension Notifications
-- Transmission of LLDP MED Extension Notification is controlled by the
-- lldpNotificationInterval object in the LLDP MIB defined in 
-- IEEE 802.1AB-2005

lldpXMedTopologyChangeDetected NOTIFICATION-TYPE
     OBJECTS { lldpRemChassisIdSubtype,
               lldpRemChassisId,
               lldpXMedRemDeviceClass
               }
           STATUS current
DESCRIPTION
               "A notification generated by the local device sensing
                a change in the topology that indicates that a new remote
                device attached to a local port, or a remote device disconnected 
                or moved from one port to another."
           ::= { lldpXMedNotifications 1 }


-- LLDP MED extension MIB groups

lldpXMedConfig     OBJECT IDENTIFIER ::= { lldpXMedObjects 1 }
lldpXMedLocalData  OBJECT IDENTIFIER ::= { lldpXMedObjects 2 }
lldpXMedRemoteData OBJECT IDENTIFIER ::= { lldpXMedObjects 3 }

-- textual conventions

LldpXMedDeviceClass  ::= TEXTUAL-CONVENTION
    STATUS     current
    DESCRIPTION
            "Device Class to which the device is a member.  

            A value of notDefined(0) indicates that the device 
            has capabilities not covered by any of the LLDP-MED classes. 
            
            A value of endpointClass1(1) indicates that the device 
            has endpoint class 1 capabilities. 
            
            A value of endpointClass2(2) indicates that the device 
            has endpoint class 2 capabilities. 
            
            A value of endpointClass3(3) indicates that the device 
            has endpoint class 3 capabilities. 
            
            A value of networkConnectivity(4) indicates that the device 
            has network connectivity device capabilities. 
            "
    
    SYNTAX      INTEGER {
            notDefined(0),
            endpointClass1(1),
            endpointClass2(2),
            endpointClass3(3),
            networkConnectivity(4)
    }

-- LLDP-MED Capabilities TC

LldpXMedCapabilities  ::= TEXTUAL-CONVENTION
    STATUS     current
    DESCRIPTION
            "Bitmap that includes the MED organizationally defined set of LLDP
            TLVs the device is capable of and whose transmission is allowed on 
            the local LLDP agent by network management.  

            Each bit in the bitmap corresponds to an LLDP-MED subtype associated  
            with a specific TIA TR41.4 MED TLV.  

            Having the bit 'capabilities(0)' set indicates that the LLDP 
            agent refers to the Capabilities TLVs.

            Having the bit 'networkPolicy(1)' set indicates that the LLDP 
            agent refers to the Network Policy TLVs.

            Having the bit 'location(2)' set indicates that 
            the LLDP agent refers to the Emergency Communications
            System Location TLVs.

            Having the bit 'extendedPSE(3)' set indicates that 
            the LLDP agent refers to the Extended PoE TLVs with PSE 
            capabilities.

            Having the bit 'extendedPD(4)' set indicates that 
            the LLDP agent refers to the Extended PoE TLVs with PD 
            capabilities.

            Having the bit 'inventory(5)' set indicates that 
            the LLDP agent refers to the Hardware Revision, Firmware 
            Revision, Software Revision, Serial Number, Manufacturer Name, 
            Model Name, and Asset ID TLVs."
    
    SYNTAX      BITS {
            capabilities(0),
            networkPolicy(1),
            location(2),
            extendedPSE(3),
            extendedPD(4),
            inventory(5)
    }


--  Location Subtype Textual Convention

LocationSubtype ::= TEXTUAL-CONVENTION 
    STATUS      current
    DESCRIPTION
            "The location subtype advertised by the remote endpoint.

             A value coordinateBased(2) indicates that the location subtype
             advertised by the endpoint is defined to use the relevant sub-
             fields of the DHCP option for Coordinate LCI as specified in 
             ANSI/TIA-1057, Section 10.2.4.3.1.

             A value civicAddress(3) indicates that the location subtype
             advertised by the endpoint is defined to use the relevant sub-
             fields of the DHCP option for Civic Address as specified in 
             ANSI/TIA-1057, Section 10.2.4.3.2.

             A value elin(4) indicates that the location subtype 
             advertised by the endpoint is defined to use the Emergency 
             Location Information Number (ELIN) as specified in
             ANSI/TIA-1057, Section 10.2.4.3.3."
    SYNTAX      INTEGER  {
                    unknown(1),
                    coordinateBased(2),
                    civicAddress(3),
                    elin(4)
                }

-- Policy Application Type Textual Convention

PolicyAppType ::= TEXTUAL-CONVENTION
    STATUS      current
    DESCRIPTION
            "The media type that defines the primary function of the
             application for the policy advertised by an endpoint.

             Having the bit voice(1) set indicates that the media type defining
             a primary function of the application for the policy advertised on 
             the local port is voice. 

             Having the bit voiceSignaling(3) set indicates that the media type 
             defining a primary function of the application for the policy 
             advertised on the local port is voice signaling. 

             Having the bit guestVoice(4) set indicates that the media type 
             Defining a primary function of the application for the policy            
             advertised on the local port is guest voice. 

             Having the bit guestVoiceSignaling(5) set indicates that the media
             type defining a primary function of the application for the policy 
             advertised on the local port is guest voice signaling. 

             Having the bit softPhoneVoice(6) set indicates that the media type 
             Defining a primary function of the application for the policy 
             advertised on the local port is softphone voice. 

             Having the bit videoConferencing(7) set indicates that the media 
             type defining a primary function of the application for the policy 
             advertised on the local port is voice. 

             Having the bit streamingVideo(8) set indicates that the media type 
             defining a primary function of the application for the policy 
             advertised on  the local port is streaming video. 

             Having the bit videoSignaling(2) set indicates that the media type 
             defining a primary function of the application for the policy 
             advertised on the local port is video signaling."
    SYNTAX      BITS  {
                    unknown(0),
                    voice(1),
                    voiceSignaling(2),
                    guestVoice(3),
                    guestVoiceSignaling(4),
                    softPhoneVoice(5),
                    videoconferencing(6),
                    streamingVideo(7),
                    videoSignaling(8)
                }

    
------------------------------------------------------------------------------
-- MED - Configuration
------------------------------------------------------------------------------

lldpXMedLocDeviceClass    OBJECT-TYPE
    SYNTAX      LldpXMedDeviceClass
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Local Device Class."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.2.2"
    ::= { lldpXMedConfig 1 }


lldpXMedPortConfigTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedPortConfigEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "A table that controls selection of LLDP TLVs to be transmitted 
            on individual ports."
    ::= { lldpXMedConfig 2 }

lldpXMedPortConfigEntry  OBJECT-TYPE
    SYNTAX      LldpXMedPortConfigEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "LLDP configuration information that controls the
            transmission of the MED organizationally defined TLVs on
            LLDP transmission capable ports.

            This configuration object augments the lldpPortConfigEntry of
            the LLDP-MIB, therefore it is only present along with the port
            configuration defined by the associated lldpPortConfigEntry
            entry.

            Each active lldpXMedPortConfigEntry must be stored and 
            retrieved from non-volatile storage (along with the 
            corresponding lldpPortConfigEntry) after a re-initialization 
            of the management system."
    AUGMENTS { lldpPortConfigEntry }
    ::= { lldpXMedPortConfigTable 1 }

LldpXMedPortConfigEntry ::= SEQUENCE {
    lldpXMedPortCapSupported        LldpXMedCapabilities,  
    lldpXMedPortConfigTLVsTxEnable  LldpXMedCapabilities,
    lldpXMedPortConfigNotifEnable   TruthValue 
}

lldpXMedPortCapSupported  OBJECT-TYPE
    SYNTAX      LldpXMedCapabilities
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The bitmap includes the MED organizationally defined set of LLDP
            TLVs whose transmission is possible for the respective port
            on the LLDP agent of the device. Each bit in the bitmap corresponds
            to an LLDP-MED subtype associated with a specific TIA TR41.4 MED 
            optional TLV. If the bit is set, the agent supports the 
            corresponding TLV."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.2.3"
    ::= { lldpXMedPortConfigEntry  1 }

lldpXMedPortConfigTLVsTxEnable  OBJECT-TYPE
    SYNTAX      LldpXMedCapabilities
    MAX-ACCESS  read-write
    STATUS      current
    DESCRIPTION
            "The lldpXMedPortConfigTLVsTxEnable, defined as a bitmap,
            includes the MED organizationally defined set of LLDP
            TLVs whose transmission is allowed on the local LLDP agent by
            the network management.  Each bit in the bitmap corresponds
            to an LLDP-MED subtype associated with a specific TIA TR41.4 MED 
            optional TLV. If the bit is set, the agent will send the 
            corresponding TLV if the respective capability is supported per 
            port.

            Setting a bit with in this object for a non-supported capability
            shall have no functional effect and will result in an inconsistent
            value error returned to the management application. 
 
            There are other rules and restrictions that prevent arbitrary
            combinations of TLVs to be enabled on LLDP-MED devices according to
            the device classes. These rules are defined in Section 10.2.1, 
            Tables 5 - 9 of ANSI/TIA-1057. In case a management application 
            attempts to set this object to a value that does not follow the rules, 
            the set operation shall have and will result in an inconsistent 
            value error returned to the management application. 

            Setting this object to an empty set is valid and effectively 
            disables LLDP-MED on a per-port basis by disabling transmission of 
            all MED organizational TLVs. In this case the remote tables objects 
            in the LLDP-MED MIB corresponding to the respective port will not 
            be populated. 
             
            The default value for lldpXMedPortConfigTLVsTxEnable object
            is an empty set, which means no enumerated values are set.

            The value of this object must be restored from non-volatile
            storage after a re-initialization of the management system."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.2.3"
    DEFVAL  { { } }
    ::= { lldpXMedPortConfigEntry  2 }

lldpXMedPortConfigNotifEnable    OBJECT-TYPE
    SYNTAX      TruthValue
    MAX-ACCESS  read-write
    STATUS      current
    DESCRIPTION
            "A value of 'true(1)' enables sending the topology change 
             traps on this port.
             A value of 'false(2)' disables sending the topology change 
             traps on this port."
    REFERENCE 
            " ANSI/TIA-1057, Section 12.3"
    DEFVAL   { false }
    ::= { lldpXMedPortConfigEntry 3 }



lldpXMedFastStartRepeatCount    OBJECT-TYPE
    SYNTAX      Unsigned32 (1..10)
    MAX-ACCESS  read-write
    STATUS      current
    DESCRIPTION
            "The number of times the fast start LLDPDU are being sent during the 
             activation of the fast start mechanism defined by LLDP-MED."
    REFERENCE 
            " ANSI/TIA-1057, Section 11.2.1"
    DEFVAL   { 3 }
    ::= { lldpXMedConfig 3 }




------------------------------------------------------------------------------
-- LLDP-MED - Local Device Information 
------------------------------------------------------------------------------
---
--- lldpXMedLocMediaPolicyTable: Local Media Policy
---                        Information Table
---
---
lldpXMedLocMediaPolicyTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedLocMediaPolicyEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains one row per policy type per port 
             of media policy information (as a part of the MED 
             organizational extension) on the local system known 
             to this agent."
    ::= { lldpXMedLocalData 1 }
 
lldpXMedLocMediaPolicyEntry OBJECT-TYPE
    SYNTAX      LldpXMedLocMediaPolicyEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about a particular policy on a specific 
             port component."
    INDEX   { lldpLocPortNum, lldpXMedLocMediaPolicyAppType }
    ::= { lldpXMedLocMediaPolicyTable 1 }
 
LldpXMedLocMediaPolicyEntry ::= SEQUENCE {
              lldpXMedLocMediaPolicyAppType        PolicyAppType,
              lldpXMedLocMediaPolicyVlanID         Integer32,
              lldpXMedLocMediaPolicyPriority       Integer32, 
              lldpXMedLocMediaPolicyDscp           Dscp,
              lldpXMedLocMediaPolicyUnknown        TruthValue,
              lldpXMedLocMediaPolicyTagged         TruthValue
} 

lldpXMedLocMediaPolicyAppType OBJECT-TYPE
    SYNTAX      PolicyAppType
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "The media type that defines the primary function of the
             application for the policy advertised by an endpoint."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.3.1"
    ::= { lldpXMedLocMediaPolicyEntry 1 }

lldpXMedLocMediaPolicyVlanID  OBJECT-TYPE
    SYNTAX      Integer32 (0|1..4094|4095)
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "An extension of the VLAN Identifier for the port, 
             as defined in IEEE 802.1P-1998.
  
             A value of 1 through 4094 is used to define a valid PVID.
  
             A value of 0 shall be used if the device is using priority tagged
             frames, meaning that only the 802.1p priority level is significant
             and the default VID of the ingress port is being used instead.
  
             A value of 4095 is reserved for implementation use."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.5"
    ::= { lldpXMedLocMediaPolicyEntry 2 }

lldpXMedLocMediaPolicyPriority  OBJECT-TYPE
    SYNTAX      Integer32 (0..7)
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the 802.1p priority
            which is associated with the given port on the
            local system."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.6 "
    ::= { lldpXMedLocMediaPolicyEntry 3 }

lldpXMedLocMediaPolicyDscp  OBJECT-TYPE
    SYNTAX 	    Dscp
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the Differentiated Service
            Code Point (DSCP) as defined in IETF RFC 2474 and RFC 2475
            which is associated with the given port on the local system."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.7"
    ::= { lldpXMedLocMediaPolicyEntry 4 }

lldpXMedLocMediaPolicyUnknown  OBJECT-TYPE
    SYNTAX 	    TruthValue
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "A value of 'true' indicates that the 
             network policy for the specified application type is 
             currently unknown.  In this case, the VLAN ID, the 
             layer 2 priority and the DSCP value fields are ignored.
             A value of 'false' indicates that this network policy 
             is defined  "
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.2"
    ::= { lldpXMedLocMediaPolicyEntry 5 }

lldpXMedLocMediaPolicyTagged  OBJECT-TYPE
    SYNTAX 	    TruthValue
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "A value of 'true' indicates that the application is using a 
             tagged VLAN.
             A value of 'false' indicates that for the specific application
             the device either is using an untagged VLAN or does not 
             support port based VLAN operation.  In this case, both the 
             VLAN ID and the Layer 2 priority fields are ignored and 
             only the DSCP value has relevance "
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.3"
    ::= { lldpXMedLocMediaPolicyEntry 6 }



--- Inventory Information
--- Local Inventory Information transmitted by an endpoint

lldpXMedLocHardwareRev    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific hardware revision string
            as advertised by the endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.1"
    ::= { lldpXMedLocalData 2 }

lldpXMedLocFirmwareRev    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific firmware revision string
            as advertised by the endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.2"
    ::= { lldpXMedLocalData 3 }

lldpXMedLocSoftwareRev    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific software revision string
            as advertised by the endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.3"
    ::= { lldpXMedLocalData 4 }

lldpXMedLocSerialNum    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific serial number
            as advertised by the endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.4"
    ::= { lldpXMedLocalData 5 }

lldpXMedLocMfgName    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific manufacturer name
            as advertised by the endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.5"
    ::= { lldpXMedLocalData 6 }

lldpXMedLocModelName    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific model name
            as advertised by the endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.6"
    ::= { lldpXMedLocalData 7 }

lldpXMedLocAssetID    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific asset tracking identifier
            as advertised by the endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.7"
    ::= { lldpXMedLocalData 8 }



--- Location Information
--- Local Location Information transmitted by an endpoint
--- lldpXMedLocLocationTable - Location Information
---

lldpXMedLocLocationTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedLocLocationEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains Location information as advertised
            by the local system.

            The information may be configured per port by a Location 
            Information Server (LIS) or other management application. 
            
            Multiple Location TLVs of different subtypes may be transmitted
            in the same PDU.

            The information in this table MUST be stored in non-volatile-memory 
            and persist over restart/reboot sequences."
    ::= { lldpXMedLocalData 9 }

lldpXMedLocLocationEntry OBJECT-TYPE
    SYNTAX      LldpXMedLocLocationEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about Location information for the local device." 
    INDEX   { lldpLocPortNum, lldpXMedLocLocationSubtype}
    ::= { lldpXMedLocLocationTable 1 }

LldpXMedLocLocationEntry ::= SEQUENCE {
              lldpXMedLocLocationSubtype    LocationSubtype,
              lldpXMedLocLocationInfo       OCTET STRING
              } 



lldpXMedLocLocationSubtype OBJECT-TYPE
    SYNTAX      LocationSubtype
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "The location subtype advertised by the local device."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.4.2"
    ::= { lldpXMedLocLocationEntry 1 }


lldpXMedLocLocationInfo OBJECT-TYPE
    SYNTAX      OCTET STRING (SIZE (0..256))
    MAX-ACCESS  read-write
    STATUS      current
    DESCRIPTION
            "The location information. Parsing of this information is 
             dependent upon the location subtype, as defined by the value of the 
             lldpXMedLocLocationSubtype object. "
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.4.3"
    DEFVAL { "" } 
    ::= { lldpXMedLocLocationEntry 2 }

--- Extended Power over Ethernet objects
--- 

lldpXMedLocXPoEDeviceType OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    pseDevice(2),
                    pdDevice(3),
                    none(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the type of Power-via-MDI (Power over Ethernet) advertised
             by the local device.

             A value pseDevice(2) indicates that the device is advertised as a 
             Power Sourcing Entity (PSE).

             A value pdDevice(3) indicates that the device is advertised as a 
             Powered Device (PD).

             A value of none(4) indicates that the device does not support PoE."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.1"
    ::= { lldpXMedLocalData 10 }

--- Extended PoE - PSE objects



--- PSE Port Table
 
lldpXMedLocXPoEPSEPortTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedLocXPoEPSEPortEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains one row per port of PSE PoE
            information on the local system known to this agent."
    ::= { lldpXMedLocalData 11 }
 
lldpXMedLocXPoEPSEPortEntry OBJECT-TYPE
    SYNTAX      LldpXMedLocXPoEPSEPortEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about a particular port PoE information."
    INDEX   { lldpLocPortNum }
    ::= { lldpXMedLocXPoEPSEPortTable 1 }
 
LldpXMedLocXPoEPSEPortEntry ::= SEQUENCE {
              lldpXMedLocXPoEPSEPortPowerAv           Gauge32,
              lldpXMedLocXPoEPSEPortPDPriority        INTEGER
} 
 
lldpXMedLocXPoEPSEPortPowerAv  OBJECT-TYPE
    SYNTAX      Gauge32 (0..1023)
    UNITS      "tenth of watt"
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the power available from the
            PSE via this port expressed in units of 0.1 watts."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.5.4 "
    ::= { lldpXMedLocXPoEPSEPortEntry 1 }
 
lldpXMedLocXPoEPSEPortPDPriority OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    critical(2),
                    high(3),
                    low(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Reflects the PD power priority that is being advertised on this
             PSE port.

             If both locally configure priority and 
             ldpXMedRemXPoEPDPowerPriority are available on this port, it is
             a matter of local policy which one takes precedence. This object 
             reflects the active value on this port. 
 
             If the priority is not configured or known by the PD, the value 
             unknown(1) will be returned. 
       
             A value critical(2) indicates that the device advertises its power 
             Priority as critical, as per RFC 3621.
 
             A value high(3) indicates that the device advertises its power 
             Priority as high, as per RFC 3621.
 
             A value low(4) indicates that the device advertises its power 
             Priority as low, as per RFC 3621."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.3"
    ::= { lldpXMedLocXPoEPSEPortEntry 2 }
 
 

lldpXMedLocXPoEPSEPowerSource OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    primary(2),
                    backup(3)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the type of PSE Power Source advertised
             by the local device.

             A value primary(2) indicates that the device advertises its power 
             source as primary.

             A value backup(3) indicates that the device advertises its power 
             Source as backup."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.2"
    ::= { lldpXMedLocalData 12 }


--- Extended PoE - PD objects

lldpXMedLocXPoEPDPowerReq  OBJECT-TYPE
    SYNTAX      Gauge32 (0..1023)
    UNITS      "tenth of watt" 
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the power required by a 
            PD expressed in units of 0.1 watts."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.4.3 "
    ::= { lldpXMedLocalData 13 }

lldpXMedLocXPoEPDPowerSource OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    fromPSE(2),
                    local(3),
                    localAndPSE(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the type of Power Source advertised as being used 
             by the local device.

             A value fromPSE(2) indicates that the device advertises its power 
             source as received from a PSE.

             A value local(3) indicates that the device advertises its power 
             source as local.

             A value localAndPSE(4) indicates that the device advertises its 
             power source as using both local and PSE power."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.2"
    ::= { lldpXMedLocalData 14 }

lldpXMedLocXPoEPDPowerPriority OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    critical(2),
                    high(3),
                    low(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the priority advertised as being required by this PD.

             A value critical(2) indicates that the device advertises its power 
             Priority as critical, as per RFC 3621.

             A value high(3) indicates that the device advertises its power 
             Priority as high, as per RFC 3621.

             A value low(4) indicates that the device advertises its power 
             Priority as low, as per RFC 3621."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.3"
    ::= { lldpXMedLocalData 15 }



------------------------------------------------------------------------------
-- LLDP-MED  - Remote Devices Information
------------------------------------------------------------------------------



-- LLdpXMedRemCapabilitiesTable
-- this table is read by a manager to determine what capabilities
-- exists and are enabled on the remote system connected to the port
 
-- The information in this table is based upon the information advertised 
-- by the remote device and received on each port in the capabilities TLV
 
lldpXMedRemCapabilitiesTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedRemCapabilitiesEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "A table that displays LLDP-MED capabilities of remote devices 
            connected to individual ports."
    ::= { lldpXMedRemoteData 1 }

lldpXMedRemCapabilitiesEntry  OBJECT-TYPE
    SYNTAX      LldpXMedRemCapabilitiesEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "LLDP-MED capabilities of remote devices connected to the device 
            ports and communicating via LLDP-MED.

            The remote tables in the LLDP-MED MIB excepting this table may be 
            sparsely populate. An entry in one of these table is meaningful 
            and shall be populated by the agent only if the corresponding bits
            for the respective function are set in the objects in this table. "
    INDEX   { lldpRemTimeMark,
              lldpRemLocalPortNum,
              lldpRemIndex }
    ::= { lldpXMedRemCapabilitiesTable 1 }

LldpXMedRemCapabilitiesEntry ::= SEQUENCE {
      lldpXMedRemCapSupported  LldpXMedCapabilities,
      lldpXMedRemCapCurrent    LldpXMedCapabilities,
      lldpXMedRemDeviceClass   LldpXMedDeviceClass 
}

lldpXMedRemCapSupported  OBJECT-TYPE
    SYNTAX      LldpXMedCapabilities
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The bitmap includes the MED organizationally defined set of LLDP
            TLVs whose transmission is possible on the LLDP agent of the remote
            device connected to this port. Each bit in the bitmap corresponds
            to an LLDP-MED subtype associated with a specific TIA TR41.4 MED                
            optional TLV. If the bit is set, the agent has the capability 
            to support the corresponding TLV."
    REFERENCE 
            "ANSI/TIA-1057, Sections 10.2.2.1"
    ::= { lldpXMedRemCapabilitiesEntry  1 }

lldpXMedRemCapCurrent  OBJECT-TYPE
    SYNTAX      LldpXMedCapabilities
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The bitmap includes the MED organizationally defined set of LLDP
            TLVs whose transmission is possible on the LLDP agent of the remote
            device connected to this port. Each bit in the bitmap corresponds
            to an LLDP-MED subtype associated with a specific TIA TR41.4 MED                
            optional TLV. If the bit is set, the agent currently supports the 
            corresponding TLV."
    REFERENCE 
            "ANSI/TIA-1057, Sections 10.2.2.1"
    ::= { lldpXMedRemCapabilitiesEntry  2 }

lldpXMedRemDeviceClass    OBJECT-TYPE
    SYNTAX      LldpXMedDeviceClass
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Device Class as advertised by the device remotely connected to the 
             port."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.2.2"
    ::= { lldpXMedRemCapabilitiesEntry 3 }




---
---
--- lldpXMedRemMediaPolicyTable: Media Policy Table
---
---
lldpXMedRemMediaPolicyTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedRemMediaPolicyEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains media policy information as advertised
            by the remote system.

            This table may be sparsely populated. Entries in this table are
            relevant only if the networkPolicy(0) bits in the 
            lldpXMedRemCapSupported and lldpXMedRemCapCurrent objects of the 
            corresponding ports are set."
    ::= { lldpXMedRemoteData 2 }

lldpXMedRemMediaPolicyEntry OBJECT-TYPE
    SYNTAX      LldpXMedRemMediaPolicyEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about the per port per policy type policy 
             information for a particular physical network connection."
    INDEX   { lldpRemTimeMark,
              lldpRemLocalPortNum,
              lldpRemIndex, 
              lldpXMedRemMediaPolicyAppType }
    ::= { lldpXMedRemMediaPolicyTable 1 }
 

LldpXMedRemMediaPolicyEntry ::= SEQUENCE {
              lldpXMedRemMediaPolicyAppType        PolicyAppType,
              lldpXMedRemMediaPolicyVlanID         Integer32,
              lldpXMedRemMediaPolicyPriority       Integer32, 
              lldpXMedRemMediaPolicyDscp           Dscp,
              lldpXMedRemMediaPolicyUnknown        TruthValue,
              lldpXMedRemMediaPolicyTagged         TruthValue
}

lldpXMedRemMediaPolicyAppType OBJECT-TYPE
    SYNTAX      PolicyAppType
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "The media type that defines the primary function of the
             application for the policy advertised by the endpoint connected 
             remotely to this port." 
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.3.1"
    ::= { lldpXMedRemMediaPolicyEntry 1 }

lldpXMedRemMediaPolicyVlanID  OBJECT-TYPE
    SYNTAX      Integer32 (0|1..4094|4095)
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "An extension of the VLAN Identifier for the remote system
             connected to this port, as defined in IEEE 802.1P-1998.
             
             A value of 1 through 4094 is used to define a valid PVID.
             
             A value of 0 shall be used if the device is using priority tagged
             frames, meaning that only the 802.1p priority level is significant
             and the default VID of the ingress port is being used instead.
             
             A value of 4095 is reserved for implementation use."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.5"
    ::= { lldpXMedRemMediaPolicyEntry 2 }

lldpXMedRemMediaPolicyPriority  OBJECT-TYPE
    SYNTAX      Integer32 (0..7)
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the 802.1p priority
            which is associated with the remote system connected at
            given port."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.6"
    ::= { lldpXMedRemMediaPolicyEntry 3 }

lldpXMedRemMediaPolicyDscp  OBJECT-TYPE
    SYNTAX 	    Dscp
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the Differentiated Service
            Code Point (DSCP) as defined in IETF RFC 2474 and RFC 2475
            which is associated with remote system connected at the port."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.7"
    ::= { lldpXMedRemMediaPolicyEntry 4 }

lldpXMedRemMediaPolicyUnknown  OBJECT-TYPE
    SYNTAX 	    TruthValue
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "A value of 'true' indicates that the 
             network policy for the specified application type is 
             currently unknown.  In this case, the VLAN ID, the 
             layer 2 priority and the DSCP value fields are ignored.
             A value of 'false' indicates that this network policy 
             is defined."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.2"
    ::= { lldpXMedRemMediaPolicyEntry 5 }

lldpXMedRemMediaPolicyTagged  OBJECT-TYPE
    SYNTAX 	    TruthValue
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "A value of 'true' indicates that the application is using a 
             tagged VLAN.
             A value of 'false' indicates that for the specific application
             the device either is using an untagged VLAN or does not 
             support port based VLAN operation.  In this case, both the 
             VLAN ID and the Layer 2 priority fields are ignored and 
             only the DSCP value has relevance "
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.3.3"
    ::= { lldpXMedRemMediaPolicyEntry 6 }




--- lldpXMedRemInventoryTable - Remote Inventory Information
--- 

lldpXMedRemInventoryTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedRemInventoryEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains inventory information as advertised
            by the remote system.
            
            This table may be sparsely populated. Entries in this table are
            relevant only if the inventory(2) bits in the 
            lldpXMedRemCapSupported and lldpXMedRemCapCurrent objects of the 
            corresponding ports are set "
    ::= { lldpXMedRemoteData 3 }

lldpXMedRemInventoryEntry OBJECT-TYPE
    SYNTAX      LldpXMedRemInventoryEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about inventory information for the remote devices
             connected to the ports." 
    INDEX   { lldpRemTimeMark,
              lldpRemLocalPortNum,
              lldpRemIndex }
    ::= { lldpXMedRemInventoryTable 1 }

LldpXMedRemInventoryEntry ::= SEQUENCE {
              lldpXMedRemHardwareRev           SnmpAdminString,
              lldpXMedRemFirmwareRev           SnmpAdminString,
              lldpXMedRemSoftwareRev           SnmpAdminString,
              lldpXMedRemSerialNum             SnmpAdminString,
              lldpXMedRemMfgName               SnmpAdminString,
              lldpXMedRemModelName             SnmpAdminString,
              lldpXMedRemAssetID               SnmpAdminString
              } 

lldpXMedRemHardwareRev    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific hardware revision string
            as advertised by the remote endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.1"
    ::= { lldpXMedRemInventoryEntry 1 }

lldpXMedRemFirmwareRev    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific firmware revision string
            as advertised by the remote endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.2"
    ::= { lldpXMedRemInventoryEntry 2 }

lldpXMedRemSoftwareRev    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific software revision string
            as advertised by the remote endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.3"
    ::= { lldpXMedRemInventoryEntry 3 }

lldpXMedRemSerialNum    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific serial number
            as advertised by the remote endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.4"
    ::= { lldpXMedRemInventoryEntry 4 }

lldpXMedRemMfgName    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific manufacturer name
            as advertised by the remote endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.5"
    ::= { lldpXMedRemInventoryEntry 5 }

lldpXMedRemModelName    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific model name
            as advertised by the remote endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.6"
    ::= { lldpXMedRemInventoryEntry 6 }

lldpXMedRemAssetID    OBJECT-TYPE
    SYNTAX      SnmpAdminString (SIZE (0..32))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The vendor-specific asset tracking identifier
            as advertised by the remote endpoint."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.6.7"
    ::= { lldpXMedRemInventoryEntry 7 }


--- lldpXMedRemLocationTable - Remote Location Information
---

lldpXMedRemLocationTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedRemLocationEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains Location information as advertised
            by the remote system.
            
            This table may be sparsely populated. Entries in this table are
            relevant only if the Location(3) bits in the 
            lldpXMedRemCapSupported and lldpXMedRemCapCurrent objects of the 
            corresponding ports are set "
    ::= { lldpXMedRemoteData 4 }

lldpXMedRemLocationEntry OBJECT-TYPE
    SYNTAX      LldpXMedRemLocationEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about Location information for the remote devices
             connected to the ports." 
    INDEX   { lldpRemTimeMark,
              lldpRemLocalPortNum,
              lldpRemIndex,
              lldpXMedRemLocationSubtype}
    ::= { lldpXMedRemLocationTable 1 }

LldpXMedRemLocationEntry ::= SEQUENCE {
              lldpXMedRemLocationSubtype    LocationSubtype,
              lldpXMedRemLocationInfo       OCTET STRING
              } 


lldpXMedRemLocationSubtype OBJECT-TYPE
    SYNTAX      LocationSubtype
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "The location subtype advertised by the remote endpoint."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.4.2 "
    ::= { lldpXMedRemLocationEntry 1 }


lldpXMedRemLocationInfo OBJECT-TYPE
    SYNTAX      OCTET STRING (SIZE (0..256))
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The location information advertised by the remote endpoint.
             Parsing of this information is dependent upon the location  
             subtype, as defined by the value of the corresponding
             lldpXMedRemLocationSubType object. "
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.4.3 "
    ::= { lldpXMedRemLocationEntry 2 }


--- lldpXMedRemXPoETable - Information about Remote PoE Device Type
---

lldpXMedRemXPoETable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedRemXPoEEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains information about the PoE device type
            as advertised by the remote system.
            
            This table is densely populated."
    ::= { lldpXMedRemoteData 5 }

lldpXMedRemXPoEEntry OBJECT-TYPE
    SYNTAX      LldpXMedRemXPoEEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about PoE type of the remote devices
             connected to the ports." 
    INDEX   { lldpRemTimeMark,
              lldpRemLocalPortNum,
              lldpRemIndex }
    ::= { lldpXMedRemXPoETable 1 }

LldpXMedRemXPoEEntry ::= SEQUENCE {
              lldpXMedRemXPoEDeviceType    INTEGER 
              } 


lldpXMedRemXPoEDeviceType OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    pseDevice(2),
                    pdDevice(3),
                    none(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the type of Power-via-MDI (Power over Ethernet) advertised
             by the remote device.

             A value pseDevice(2) indicates that the device is advertised as a 
             Power Sourcing Entity (PSE).

             A value pdDevice(3) indicates that the device is advertised as a 
             Powered Device (PD).

             A value none(4) indicates that the device does not support PoE."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.1"
    ::= { lldpXMedRemXPoEEntry 1 }


--- lldpXMedRemXPoEPDTable - Extended PoE PSE Information from the remote device
---

lldpXMedRemXPoEPSETable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedRemXPoEPSEEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains extended PoE information as advertised
            by the remote devices of PSE type.
            
            This table may be sparsely populated. Entries in this table are
            relevant only if the extendedPSE(4) bits in the 
            lldpXMedRemCapSupported and lldpXMedRemCapCurrent objects of the 
            corresponding ports are set "
    ::= { lldpXMedRemoteData 6 }

lldpXMedRemXPoEPSEEntry OBJECT-TYPE
    SYNTAX      LldpXMedRemXPoEPSEEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about Extended PoE PSE information for 
            the remote devices connected to the ports." 
    INDEX   { lldpRemTimeMark,
              lldpRemLocalPortNum,
              lldpRemIndex }
    ::= { lldpXMedRemXPoEPSETable 1 }

LldpXMedRemXPoEPSEEntry ::= SEQUENCE {
              lldpXMedRemXPoEPSEPowerAv    Gauge32,
              lldpXMedRemXPoEPSEPowerSource INTEGER,
              lldpXMedRemXPoEPSEPowerPriority INTEGER
              } 
 

lldpXMedRemXPoEPSEPowerAv  OBJECT-TYPE
    SYNTAX      Gauge32 (0..1023)
    UNITS      "tenth of watt"
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the power available from the
            PSE via this port expressed in units of 0.1 watts on the remote 
            device."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.5.4"
    ::= { lldpXMedRemXPoEPSEEntry 1 }

lldpXMedRemXPoEPSEPowerSource OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    primary(2),
                    backup(3)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the type of PSE Power Source advertised
             by the remote device.

             A value primary(2) indicates that the device advertises its power 
             source as primary.

             A value backup(3) indicates that the device advertises its power 
             Source as backup."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.2"
    ::= { lldpXMedRemXPoEPSEEntry 2 }

lldpXMedRemXPoEPSEPowerPriority OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    critical(2),
                    high(3),
                    low(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the PSE power priority 
            advertised by the remote device.
            
            A value critical(2) indicates that the device advertises its power 
            priority as critical, as per RFC 3621.
            
            A value high(3) indicates that the device advertises its power 
            priority as high, as per RFC 3621.
            
            A value low(4) indicates that the device advertises its power 
            priority as low, as per RFC 3621."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.3"
    ::= { lldpXMedRemXPoEPSEEntry 3 }
 
 


--- lldpXMedRemXPoEPDTable - Extended PoE PD Information from the remote device
---

lldpXMedRemXPoEPDTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF LldpXMedRemXPoEPDEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains extended PoE information as advertised
            by the remote devices of PD type.
            
            This table may be sparsely populated. Entries in this table are
            relevant only if the extendedPD(5) bits in the 
            lldpXMedRemCapSupported and lldpXMedRemCapCurrent objects of the 
            corresponding ports are set "
    ::= { lldpXMedRemoteData 7 }

lldpXMedRemXPoEPDEntry OBJECT-TYPE
    SYNTAX      LldpXMedRemXPoEPDEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about XPoEPD information for the remote devices
             connected to the ports." 
    INDEX   { lldpRemTimeMark,
              lldpRemLocalPortNum,
              lldpRemIndex }
    ::= { lldpXMedRemXPoEPDTable 1 }

LldpXMedRemXPoEPDEntry ::= SEQUENCE {
              lldpXMedRemXPoEPDPowerReq       Gauge32,
              lldpXMedRemXPoEPDPowerSource    INTEGER,
              lldpXMedRemXPoEPDPowerPriority  INTEGER 
              } 


lldpXMedRemXPoEPDPowerReq  OBJECT-TYPE
    SYNTAX      Gauge32 (0..1023)
    UNITS      "tenth of watt" 
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object contains the value of the power required by a 
            PD connected remotely to the port
            expressed in units of 0.1 watts."
    REFERENCE 
            " ANSI/TIA-1057, Section 10.2.5.4 "
    ::= { lldpXMedRemXPoEPDEntry 1 }

lldpXMedRemXPoEPDPowerSource OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    fromPSE(2),
                    local(3),
                    localAndPSE(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the type of Power Source advertised as being used 
             by the device connected remotely to the port.

             A value fromPSE(2) indicates that the device advertises its power 
             source as received from a PSE.

             A value local(3) indicates that the device advertises its power 
             source as local.

             A value localAndPSE(4) indicates that the device advertises its 
             power source as using both local and PSE power."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.2"
    ::= { lldpXMedRemXPoEPDEntry 2 }

lldpXMedRemXPoEPDPowerPriority OBJECT-TYPE
    SYNTAX      INTEGER  {
                    unknown(1),
                    critical(2),
                    high(3),
                    low(4)
                }
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "Defines the priority advertised as being required by the PD
             connected remotely to the port.

             A value critical(2) indicates that the device advertises its power 
             Priority as critical, as per RFC 3621.

             A value high(3) indicates that the device advertises its power 
             Priority as high, as per RFC 3621.

             A value low(4) indicates that the device advertises its power 
             Priority as low, as per RFC 3621."
    REFERENCE 
            "ANSI/TIA-1057, Section 10.2.5.3"
    ::= { lldpXMedRemXPoEPDEntry 3 }







---


-- conformance information

lldpXMedConformance OBJECT IDENTIFIER ::= { lldpXMedMIB 2 }
lldpXMedCompliances OBJECT IDENTIFIER ::= { lldpXMedConformance 1 }
lldpXMedGroups      OBJECT IDENTIFIER ::= { lldpXMedConformance 2 }

-- compliance statements

lldpXMedCompliance MODULE-COMPLIANCE
    STATUS  current
    DESCRIPTION
            "The compliance statement for SNMP entities which implement
            the LLDP MED extension MIB."
 
    MODULE  -- this module
        MANDATORY-GROUPS { lldpXMedConfigGroup, 
                           lldpXMedRemSysGroup,
                           lldpXMedNotificationsGroup
        }
        GROUP lldpXMedOptMediaPolicyGroup
            DESCRIPTION
                "This group represents the information associated with
                the LLDP-MED optional Media Policy TLVs, 
                therefore the agent may not implement them."
        GROUP lldpXMedOptInventoryGroup
            DESCRIPTION
                "This group represents the information associated with
                the LLDP-MED optional inventory TLVs, 
                therefore the agent may not implement them."
        GROUP lldpXMedOptLocationGroup
            DESCRIPTION
                "This group represents the information associated with
                the LLDP-MED optional Location TLVs, 
                therefore the agent may not implement them."
        GROUP lldpXMedOptPoEPSEGroup
            DESCRIPTION
                "This group represents the information associated with
                the LLDP-MED optional extended PoE PolicyTLVs, carrying
                PSE information, therefore the agent may
                not implement them."
       GROUP lldpXMedOptPoEPDGroup
            DESCRIPTION
                " This group represents the information associated with
                the LLDP-MED optional extended PoE Policy TLVs, carrying
                PD information, therefore the agent may
                not implement them."
    ::= { lldpXMedCompliances 1 }

-- MIB groupings

lldpXMedConfigGroup    OBJECT-GROUP
    OBJECTS {
        lldpXMedPortCapSupported, 
        lldpXMedPortConfigTLVsTxEnable,
        lldpXMedPortConfigNotifEnable, 
        lldpXMedFastStartRepeatCount,
        lldpXMedLocXPoEDeviceType,
        lldpXMedLocDeviceClass
    }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to configure or
            describe the configuration or behavior of the LLDP-MED
            organizational extension implementation."
    ::= { lldpXMedGroups 1 }

lldpXMedOptMediaPolicyGroup  OBJECT-GROUP
    OBJECTS {
        lldpXMedLocMediaPolicyVlanID, 
        lldpXMedLocMediaPolicyPriority, 
        lldpXMedLocMediaPolicyDscp,
        lldpXMedLocMediaPolicyUnknown,
        lldpXMedLocMediaPolicyTagged  
        }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to represent LLDP
            MED organizational extensions for Media Policy Information."
    ::= { lldpXMedGroups 2 }



lldpXMedOptInventoryGroup  OBJECT-GROUP
    OBJECTS {
        lldpXMedLocHardwareRev, 
        lldpXMedLocFirmwareRev, 
        lldpXMedLocSoftwareRev, 
        lldpXMedLocSerialNum,
        lldpXMedLocMfgName,
        lldpXMedLocModelName,
        lldpXMedLocAssetID
        }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to represent LLDP
            MED organizational extension for inventory Information."
    ::= { lldpXMedGroups 3 }
lldpXMedOptLocationGroup  OBJECT-GROUP
    OBJECTS {
        lldpXMedLocLocationInfo 
        }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to represent LLDP
            MED organizational extension for Location Information."
    ::= { lldpXMedGroups 4 }


lldpXMedOptPoEPSEGroup  OBJECT-GROUP
    OBJECTS {
        lldpXMedLocXPoEPSEPortPowerAv,
        lldpXMedLocXPoEPSEPortPDPriority, 
        lldpXMedLocXPoEPSEPowerSource 
        } 
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to represent LLDP
            MED organizational extensions for PoE PSE Information."
    ::= { lldpXMedGroups 5 }

lldpXMedOptPoEPDGroup  OBJECT-GROUP
    OBJECTS {
        lldpXMedLocXPoEPDPowerReq, 
        lldpXMedLocXPoEPDPowerSource, 
        lldpXMedLocXPoEPDPowerPriority
        }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to represent LLDP
            MED organizational extensions for PoE PD Information."
    ::= { lldpXMedGroups 6 }

lldpXMedRemSysGroup  OBJECT-GROUP
    OBJECTS {
        lldpXMedRemCapSupported,
        lldpXMedRemCapCurrent,
        lldpXMedRemDeviceClass,
        lldpXMedRemMediaPolicyVlanID,
        lldpXMedRemMediaPolicyPriority,
        lldpXMedRemMediaPolicyDscp,
        lldpXMedRemMediaPolicyUnknown,
        lldpXMedRemMediaPolicyTagged,  
        lldpXMedRemHardwareRev,
        lldpXMedRemFirmwareRev,
        lldpXMedRemSoftwareRev,
        lldpXMedRemSerialNum,
        lldpXMedRemMfgName,
        lldpXMedRemModelName,
        lldpXMedRemAssetID,
        lldpXMedRemLocationInfo,
        lldpXMedRemXPoEDeviceType,
        lldpXMedRemXPoEPSEPowerAv,
        lldpXMedRemXPoEPSEPowerSource,
        lldpXMedRemXPoEPSEPowerPriority,
        lldpXMedRemXPoEPDPowerReq,
        lldpXMedRemXPoEPDPowerSource,
        lldpXMedRemXPoEPDPowerPriority 
    }
     STATUS  current
    DESCRIPTION
            "The collection of objects which are used to represent LLDP-
            MED organizational extension Remote Device Information."
    ::= { lldpXMedGroups 7 }

lldpXMedNotificationsGroup NOTIFICATION-GROUP
     NOTIFICATIONS { lldpXMedTopologyChangeDetected }
     STATUS current
     DESCRIPTION
           "Notifications sent by an LLDP-MED agent."
           ::= { lldpXMedGroups 8 }



END