User information about Rittal Visio Shapes

Rittal GmbH & Co. KG, Auf dem Sttzelberg, D-35745 Herborn, Germany

The files can be used from the VISIO 2010 release.

The Rittal VISIO shapes are always bound to the Rittal template,
this has the following advantages :
- The files and drawings harmonize with the VISIO Rack Configurator 2013
- Presentation of the cabinets with the scale 1:1
- Use of flexible dimensions width and height
- U capture function in 19" profile of the cabinets
- All 19" mounting components are Labeled
- All 19" mounting components have Properties details listed,
  which can be customized.

Start
1 Use "File" -> "Open" to select the file "Rittal_template.vsd"
2 Now open the shapes with a double click on the VSS-file.
   e.g. the file "Rittal_TS_IT_2014_03_04"
3 Drag a Rittal cabinet in the template
4 Drag the dimension in the template and adjust them.
5 You can complete the cabinet with 19" mounting components.
End