-- extracted from rfc2922.txt
-- at Fri Sep 29 07:11:06 2000

PTOPO-MIB DEFINITIONS ::= BEGIN

IMPORTS
    MODULE-IDENTITY, OBJECT-TYPE, NOTIFICATION-TYPE,
    Integer32, Counter32, mib-2
        FROM SNMPv2-SMI
    TEXTUAL-CONVENTION, AutonomousType, RowStatus, TimeStamp, TruthValue
        FROM SNMPv2-TC
    MODULE-COMPLIANCE, OBJECT-GROUP, NOTIFICATION-GROUP
        FROM SNMPv2-CONF
    TimeFilter
        FROM RMON2-MIB
    PhysicalIndex
        FROM ENTITY-MIB
    AddressFamilyNumbers
        FROM IANA-ADDRESS-FAMILY-NUMBERS-MIB;

ptopoMIB MODULE-IDENTITY
    LAST-UPDATED "200009210000Z"
    ORGANIZATION "IETF; PTOPOMIB Working Group"
    CONTACT-INFO
       "PTOPOMIB WG Discussion:
        ptopo@3com.com
        Subscription:
        majordomo@3com.com
          msg body: [un]subscribe ptopomib

        Andy Bierman
        Cisco Systems Inc.
        170 West Tasman Drive
        San Jose, CA 95134
        408-527-3711
        abierman@cisco.com

        Kendall S. Jones
        Nortel Networks
        4401 Great America Parkway
        Santa Clara, CA 95054
        408-495-7356
        kejones@nortelnetworks.com"
    DESCRIPTION
            "The MIB module for physical topology information."
    REVISION        "200009210000Z"
    DESCRIPTION
            "Initial Version of the Physical Topology MIB.  This version
            published as RFC 2922."
    ::= { mib-2 79 }

ptopoMIBObjects   OBJECT IDENTIFIER ::= { ptopoMIB 1 }


-- MIB groups
ptopoData         OBJECT IDENTIFIER ::= { ptopoMIBObjects 1 }
ptopoGeneral      OBJECT IDENTIFIER ::= { ptopoMIBObjects 2 }
ptopoConfig       OBJECT IDENTIFIER ::= { ptopoMIBObjects 3 }

-- textual conventions
PtopoGenAddr ::= TEXTUAL-CONVENTION
    STATUS      current
    DESCRIPTION
            "The value of an address."
    SYNTAX      OCTET STRING (SIZE (0..20))

PtopoChassisIdType ::= TEXTUAL-CONVENTION
    STATUS      current
    DESCRIPTION
            "This TC describes the source of a chassis identifier.

            The enumeration 'chasIdEntPhysicalAlias(1)' represents a
            chassis identifier based on the value of entPhysicalAlias
            for a chassis component (i.e., an entPhysicalClass value of
            'chassis(3)').

            The enumeration 'chasIdIfAlias(2)' represents a chassis
            identifier based on the value of ifAlias for an interface
            on the containing chassis.

            The enumeration 'chasIdPortEntPhysicalAlias(3)' represents
            a chassis identifier based on the value of entPhysicalAlias
            for a port or backplane component (i.e., entPhysicalClass
            value of 'port(10)' or 'backplane(4)'), within the
            containing chassis.

            The enumeration 'chasIdMacAddress(4)' represents a chassis
            identifier based on the value of a unicast source MAC
            address (encoded in network byte order and IEEE 802.3
            canonical bit order), of a port on the containing chassis.

            The enumeration 'chasIdPtopoGenAddr(5)' represents a
            chassis identifier based on a network address, associated
            with a particular chassis.  The encoded address is actually
            composed of two fields.  The first field is a single octet,
            representing the IANA AddressFamilyNumbers value for the
            specific address type, and the second field is the
            PtopoGenAddr address value."
    SYNTAX      INTEGER {
            chasIdEntPhysicalAlias(1),
            chasIdIfAlias(2),
            chasIdPortEntPhysicalAlias(3),
            chasIdMacAddress(4),
            chasIdPtopoGenAddr(5)
    }

PtopoChassisId ::= TEXTUAL-CONVENTION
    STATUS      current
    DESCRIPTION
            "This TC describes the format of a chassis identifier
            string.  Objects of this type are always used with an
            associated PtopoChassisIdType object, which identifies the
            format of the particular PtopoChassisId object instance.

            If the associated PtopoChassisIdType object has a value of
            'chasIdEntPhysicalAlias(1)', then the octet string
            identifies a particular instance of the entPhysicalAlias
            object for a chassis component (i.e., an entPhysicalClass
            value of 'chassis(3)').

            If the associated PtopoChassisIdType object has a value of
            'chasIdIfAlias(2)', then the octet string identifies a
            particular instance of the ifAlias object for an interface
            on the containing chassis.

            If the associated PtopoChassisIdType object has a value of
            'chasIdPortEntPhysicalAlias(3)', then the octet string
            identifies a particular instance of the entPhysicalAlias
            object for a port or backplane component within the
            containing chassis.

            If the associated PtopoChassisIdType object has a value of
            'chasIdMacAddress(4)', then this string identifies a
            particular unicast source MAC address (encoded in network
            byte order and IEEE 802.3 canonical bit order), of a port on
            the containing chassis.

            If the associated PtopoChassisIdType object has a value of
            'chasIdPtopoGenAddr(5)', then this string identifies a
            particular network address, encoded in network byte order,
            associated with one or more ports on the containing chassis.
            The first octet contains the IANA Address Family Numbers
            enumeration value for the specific address type, and octets
            2 through N contain the PtopoGenAddr address value in
            network byte order."
    SYNTAX      OCTET STRING (SIZE (1..32))

PtopoPortIdType ::= TEXTUAL-CONVENTION
    STATUS      current
    DESCRIPTION
            "This TC describes the source of a particular type of port
            identifier used in the PTOPO MIB.

            The enumeration 'portIdIfAlias(1)' represents a port
            identifier based on the ifAlias MIB object.
            The enumeration 'portIdPortEntPhysicalAlias(2)' represents a
            port identifier based on the value of entPhysicalAlias for a
            port or backplane component (i.e., entPhysicalClass value of
            'port(10)' or 'backplane(4)'), within the containing
            chassis.

            The enumeration 'portIdMacAddr(3)' represents a port
            identifier based on a unicast source MAC address, which has
            been detected by the agent and associated with a particular
            port.

            The enumeration 'portIdPtopoGenAddr(4)' represents a port
            identifier based on a network address, detected by the agent
            and associated with a particular port."
    SYNTAX      INTEGER {
            portIdIfAlias(1),
            portIdEntPhysicalAlias(2),
            portIdMacAddr(3),
            portIdPtopoGenAddr(4)
    }

PtopoPortId ::= TEXTUAL-CONVENTION
    STATUS      current
    DESCRIPTION
            "This TC describes the format of a port identifier string.
            Objects of this type are always used with an associated
            PtopoPortIdType object, which identifies the format of the
            particular PtopoPortId object instance.

            If the associated PtopoPortIdType object has a value of
            'portIdIfAlias(1)', then the octet string identifies a
            particular instance of the ifAlias object.

            If the associated PtopoPortIdType object has a value of
            'portIdEntPhysicalAlias(2)', then the octet string
            identifies a particular instance of the entPhysicalAlias
            object for a port component (i.e., entPhysicalClass value of
            'port(10)').

            If the associated PtopoPortIdType object has a value of
            'portIdMacAddr(3)', then this string identifies a particular
            unicast source MAC address associated with the port.

            If the associated PtopoPortIdType object has a value of
            'portIdPtopoGenAddr(4)', then this string identifies a
            network address associated with the port.  The first octet
            contains the IANA AddressFamilyNumbers enumeration value for
            the specific address type, and octets 2 through N contain
            the PtopoGenAddr address value in network byte order."
    SYNTAX      OCTET STRING (SIZE (1..32))


PtopoAddrSeenState ::= TEXTUAL-CONVENTION
    STATUS      current
    DESCRIPTION
            "This TC describes the state of address detection for a
            particular type of port identifier used in the PTOPO MIB.

            The enumeration 'notUsed(1)' represents an entry for which
            the particular MIB object is not applicable to the remote
            connection endpoint,

            The enumeration 'unknown(2)' represents an entry for which
            the particular address collection state is not known.

            The enumeration 'oneAddr(3)'  represents an entry for which
            exactly one source address (of the type indicated by the
            particular MIB object), has been detected.

            The enumeration 'multiAddr(4)'  represents an entry for
            which more than one source address (of the type indicated by
            the particular MIB object), has been detected.

            An agent is expected to set the initial state of the
            PtopoAddrSeenState to 'notUsed(1)' or 'unknown(2)'.

            Note that the PTOPO MIB does not restrict or specify the
            means in which the PtopoAddrSeenState is known to an agent.
            In particular, an agent may detect this information through
            configuration data, or some means other than directly
            monitoring all port traffic."
    SYNTAX      INTEGER {
            notUsed(1),
            unknown(2),
            oneAddr(3),
            multiAddr(4)
    }

--  ***********************************************************
--
--           P T O P O    D A T A     G R O U P
--
--  ***********************************************************

-- Connection Table
ptopoConnTable OBJECT-TYPE
    SYNTAX      SEQUENCE OF PtopoConnEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This table contains one or more rows per physical network
            connection known to this agent.  The agent may wish to
            ensure that only one ptopoConnEntry is present for each
            local port, or it may choose to maintain multiple
            ptopoConnEntries for the same local port.

            Entries based on lower numbered identifier types are
            preferred over higher numbered identifier types, i.e., lower
            values of the ptopoConnRemoteChassisType and
            ptopoConnRemotePortType objects."
    ::= { ptopoData 1 }

ptopoConnEntry       OBJECT-TYPE
    SYNTAX      PtopoConnEntry
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "Information about a particular physical network connection.
            Entries may be created and deleted in this table, either
            manually or by the agent, if a physical topology discovery
            process is active."
    INDEX   {
           ptopoConnTimeMark,
           ptopoConnLocalChassis,
           ptopoConnLocalPort,
           ptopoConnIndex
    }
    ::= { ptopoConnTable 1 }

PtopoConnEntry ::= SEQUENCE {
      ptopoConnTimeMark            TimeFilter,
      ptopoConnLocalChassis        PhysicalIndex,
      ptopoConnLocalPort           PhysicalIndex,
      ptopoConnIndex               Integer32,
      ptopoConnRemoteChassisType   PtopoChassisIdType,
      ptopoConnRemoteChassis       PtopoChassisId,
      ptopoConnRemotePortType      PtopoPortIdType,
      ptopoConnRemotePort          PtopoPortId,
      ptopoConnDiscAlgorithm       AutonomousType,
      ptopoConnAgentNetAddrType    AddressFamilyNumbers,
      ptopoConnAgentNetAddr        PtopoGenAddr,
      ptopoConnMultiMacSASeen      PtopoAddrSeenState,
      ptopoConnMultiNetSASeen      PtopoAddrSeenState,
      ptopoConnIsStatic            TruthValue,
      ptopoConnLastVerifyTime      TimeStamp,
      ptopoConnRowStatus           RowStatus
}

ptopoConnTimeMark  OBJECT-TYPE
    SYNTAX      TimeFilter
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "A TimeFilter for this entry.  See the TimeFilter textual
            convention in RFC 2021 to see how this works."
    ::= { ptopoConnEntry 1 }

ptopoConnLocalChassis  OBJECT-TYPE
    SYNTAX      PhysicalIndex
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "The entPhysicalIndex value used to identify the chassis
            component associated with the local connection endpoint."
    ::= { ptopoConnEntry 2 }

ptopoConnLocalPort     OBJECT-TYPE
    SYNTAX      PhysicalIndex
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "The entPhysicalIndex value used to identify the port
            component associated with the local connection endpoint."
    ::= { ptopoConnEntry 3 }

ptopoConnIndex    OBJECT-TYPE
    SYNTAX      Integer32  (1..2147483647)
    MAX-ACCESS  not-accessible
    STATUS      current
    DESCRIPTION
            "This object represents an arbitrary local integer value
            used by this agent to identify a particular connection
            instance, unique only for the indicated local connection
            endpoint.

            A particular ptopoConnIndex value may be reused in the event
            an entry is aged out and later re-learned with the same (or
            different) remote chassis and port identifiers.

            An agent is encouraged to assign monotonically increasing
            index values to new entries, starting with one, after each
            reboot.  It is considered unlikely that the ptopoConnIndex
            will wrap between reboots."
    ::= { ptopoConnEntry 4 }

ptopoConnRemoteChassisType  OBJECT-TYPE
    SYNTAX      PtopoChassisIdType
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "The type of encoding used to identify the chassis
            associated with the remote connection endpoint.

            This object may not be modified if the associated
            ptopoConnRowStatus object has a value of active(1)."
    ::= { ptopoConnEntry 5 }

ptopoConnRemoteChassis  OBJECT-TYPE
    SYNTAX      PtopoChassisId
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "The string value used to identify the chassis component
            associated with the remote connection endpoint.

            This object may not be modified if the associated
            ptopoConnRowStatus object has a value of active(1)."
    ::= { ptopoConnEntry 6 }

ptopoConnRemotePortType  OBJECT-TYPE
    SYNTAX      PtopoPortIdType
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "The type of port identifier encoding used in the associated
            'ptopoConnRemotePort' object.

            This object may not be modified if the associated
            ptopoConnRowStatus object has a value of active(1)."
    ::= { ptopoConnEntry 7 }

ptopoConnRemotePort  OBJECT-TYPE
    SYNTAX      PtopoPortId
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "The string value used to identify the port component
            associated with the remote connection endpoint.
            This object may not be modified if the associated
            ptopoConnRowStatus object has a value of active(1)."
    ::= { ptopoConnEntry 8 }

ptopoConnDiscAlgorithm OBJECT-TYPE
    SYNTAX      AutonomousType
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "An indication of the algorithm used to discover the
            information contained in this conceptual row.

            A value of ptopoDiscoveryLocal indicates this entry was
            configured by the local agent, without use of a discovery
            protocol.

            A value of { 0 0 } indicates this entry was created manually
            by an NMS via the associated RowStatus object. "
    ::= { ptopoConnEntry 9 }

ptopoConnAgentNetAddrType  OBJECT-TYPE
    SYNTAX      AddressFamilyNumbers
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "This network address type of the associated
            ptopoConnNetAddr object, unless that object contains a zero
            length string.  In such a case, an NMS application should
            ignore any returned value for this object.

            This object may not be modified if the associated
            ptopoConnRowStatus object has a value of active(1)."
    ::= { ptopoConnEntry 10 }

ptopoConnAgentNetAddr  OBJECT-TYPE
    SYNTAX      PtopoGenAddr
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "This object identifies a network address which may be used
            to reach an SNMP agent entity containing information for the
            chassis and port components represented by the associated
            'ptopoConnRemoteChassis' and 'ptopoConnRemotePort' objects.
            If no such address is known, then this object shall contain
            an empty string.

            This object may not be modified if the associated
            ptopoConnRowStatus object has a value of active(1)."
    ::= { ptopoConnEntry 11 }

ptopoConnMultiMacSASeen  OBJECT-TYPE
    SYNTAX      PtopoAddrSeenState
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object indicates if multiple unicast source MAC
            addresses have been detected by the agent from the remote
            connection endpoint, since the creation of this entry.

            If this entry has an associated ptopoConnRemoteChassisType
            and/or ptopoConnRemotePortType value other than
            'portIdMacAddr(3)', then the value 'notUsed(1)' is returned.

            Otherwise, one of the following conditions must be true:

            If the agent has not yet detected any unicast source MAC
            addresses from the remote port, then the value 'unknown(2)'
            is returned.

            If the agent has detected exactly one unicast source MAC
            address from the remote port, then the value 'oneAddr(3)' is
            returned.

            If the agent has detected more than one unicast source MAC
            address from the remote port, then the value 'multiAddr(4)'
            is returned."
    ::= { ptopoConnEntry 12 }

ptopoConnMultiNetSASeen  OBJECT-TYPE
    SYNTAX      PtopoAddrSeenState
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "This object indicates if multiple network layer source
            addresses have been detected by the agent from the remote
            connection endpoint, since the creation of this entry.

            If this entry has an associated ptopoConnRemoteChassisType
            or ptopoConnRemotePortType value other than
            'portIdGenAddr(4)' then the value 'notUsed(1)' is returned.

            Otherwise, one of the following conditions must be true:

            If the agent has not yet detected any network source
            addresses of the appropriate type from the remote port, then
            the value 'unknown(2)' is returned.
            If the agent has detected exactly one network source address
            of the appropriate type from the remote port, then the value
            'oneAddr(3)' is returned.

            If the agent has detected more than one network source
            address (of the same appropriate type) from the remote port,
            this the value 'multiAddr(4)' is returned."
    ::= { ptopoConnEntry 13 }

ptopoConnIsStatic  OBJECT-TYPE
    SYNTAX      TruthValue
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "This object identifies static ptopoConnEntries.  If this
            object has the value 'true(1)', then this entry is not
            subject to any age-out mechanisms implemented by the agent.

            If this object has the value 'false(2)', then this entry is
            subject to all age-out mechanisms implemented by the agent.

            This object may not be modified if the associated
            ptopoConnRowStatus object has a value of active(1)."
    DEFVAL { false }
    ::= { ptopoConnEntry 14 }

ptopoConnLastVerifyTime  OBJECT-TYPE
    SYNTAX      TimeStamp
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "If the associated value of ptopoConnIsStatic is equal to
            'false(2)', then this object contains the value of sysUpTime
            at the time the conceptual row was last verified by the
            agent, e.g., via reception of a topology protocol message,
            pertaining to the associated remote chassis and port.

            If the associated value of ptopoConnIsStatic is equal to
            'true(1)', then this object shall contain the value of
            sysUpTime at the time this entry was last activated (i.e.,
            ptopoConnRowStatus set to 'active(1)')."
    ::= { ptopoConnEntry 15 }

ptopoConnRowStatus OBJECT-TYPE
    SYNTAX      RowStatus
    MAX-ACCESS  read-create
    STATUS      current
    DESCRIPTION
            "The status of this conceptual row."
    ::= { ptopoConnEntry 16 }

--  ***********************************************************
--
--           P T O P O    G E N E R A L     G R O U P
--
--  ***********************************************************

-- last change time stamp for the whole MIB

ptopoLastChangeTime OBJECT-TYPE
    SYNTAX      TimeStamp
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The value of sysUpTime at the time a conceptual row is
            created, modified, or deleted in the ptopoConnTable.

            An NMS can use this object to reduce polling of the
            ptopoData group objects."
    ::= { ptopoGeneral 1 }

ptopoConnTabInserts OBJECT-TYPE
    SYNTAX      Counter32
    UNITS       "table entries"
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The number of times an entry has been inserted into the
            ptopoConnTable."
    ::= { ptopoGeneral 2 }

ptopoConnTabDeletes OBJECT-TYPE
    SYNTAX      Counter32
    UNITS       "table entries"
    MAX-ACCESS  read-only
    STATUS      current

    DESCRIPTION
            "The number of times an entry has been deleted from the
            ptopoConnTable."
    ::= { ptopoGeneral 3 }

ptopoConnTabDrops OBJECT-TYPE
    SYNTAX      Counter32
    UNITS       "table entries"
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The number of times an entry would have been added to the
            ptopoConnTable, (e.g., via information learned from a
            topology protocol), but was not because of insufficient
            resources."
    ::= { ptopoGeneral 4 }

ptopoConnTabAgeouts OBJECT-TYPE
    SYNTAX      Counter32
    MAX-ACCESS  read-only
    STATUS      current
    DESCRIPTION
            "The number of times an entry has been deleted from the
            ptopoConnTable because the information timeliness interval
            for that entry has expired."
    ::= { ptopoGeneral 5 }

--  ***********************************************************
--
--           P T O P O    C O N F I G     G R O U P
--
--  ***********************************************************

ptopoConfigTrapInterval OBJECT-TYPE
    SYNTAX      Integer32 (0 | 5..3600)
    UNITS       "seconds"
    MAX-ACCESS  read-write
    STATUS      current
    DESCRIPTION
            "This object controls the transmission of PTOPO
            notifications.

            If this object has a value of zero, then no
            ptopoConfigChange notifications will be transmitted by the
            agent.

            If this object has a non-zero value, then the agent must not
            generate more than one ptopoConfigChange trap-event in the
            indicated period, where a 'trap-event' is the transmission
            of a single notification PDU type to a list of notification
            destinations.  If additional configuration changes occur
            within the indicated throttling period, then these trap-
            events must be suppressed by the agent. An NMS should
            periodically check the value of ptopoLastChangeTime to
            detect any missed ptopoConfigChange trap-events, e.g. due to
            throttling or transmission loss.
            If notification transmission is enabled, the suggested
            default throttling period is 60 seconds, but transmission
            should be disabled by default.

            If the agent is capable of storing non-volatile
            configuration, then the value of this object must be
            restored after a re-initialization of the management
            system."
    DEFVAL { 0 }
    ::= { ptopoConfig 1 }

ptopoConfigMaxHoldTime OBJECT-TYPE
    SYNTAX      Integer32 (1..2147483647)
    UNITS       "seconds"
    MAX-ACCESS  read-write
    STATUS      current
    DESCRIPTION
            "This object specifies the desired time interval for which
            an agent will maintain dynamic ptopoConnEntries.

            After the specified number of seconds since the last time an
            entry was verified, in the absence of new verification
            (e.g., receipt of a topology protocol message), the agent
            shall remove the entry.  Note that entries may not always be
            removed immediately, but may possibly be removed at periodic
            garbage collection intervals.
            This object only affects dynamic ptopoConnEntries, i.e.  for
            which ptopoConnIsStatic equals 'false(2)'. Static entries
            are not aged out.

            Note that dynamic ptopoConnEntries may also be removed by
            the agent due to the expired timeliness of learned topology
            information (e.g., timeliness interval for a remote port
            expires).  The actual age-out interval for a given entry is
            defined by the following formula:

              age-out-time =
                min(ptopoConfigMaxHoldTime, <entry-specific hold-time>)

            where <entry-specific hold-time> is determined by the
            discovery algorithm, and may be different for each entry."
    DEFVAL { 300 }
    ::= { ptopoConfig 2 }


-- PTOPO MIB Notification Definitions
ptopoMIBNotifications  OBJECT IDENTIFIER ::= { ptopoMIB 2 }
ptopoMIBTrapPrefix     OBJECT IDENTIFIER ::=
      { ptopoMIBNotifications 0 }

ptopoConfigChange NOTIFICATION-TYPE
    OBJECTS       {
             ptopoConnTabInserts,
             ptopoConnTabDeletes,
             ptopoConnTabDrops,
             ptopoConnTabAgeouts
    }
    STATUS        current
    DESCRIPTION
            "A ptopoConfigChange notification is sent when the value of
            ptopoLastChangeTime changes. It can be utilized by an NMS to
            trigger physical topology table maintenance polls.

            Note that transmission of ptopoConfigChange notifications
            are throttled by the agent, as specified by the
            'ptopoConfigTrapInterval' object."
   ::= { ptopoMIBTrapPrefix 1 }


-- PTOPO Registration Points
ptopoRegistrationPoints  OBJECT IDENTIFIER ::= { ptopoMIB 3 }

-- values used with ptopoConnDiscAlgorithm object
ptopoDiscoveryMechanisms OBJECT IDENTIFIER ::=
      { ptopoRegistrationPoints 1 }

ptopoDiscoveryLocal      OBJECT IDENTIFIER ::=
      { ptopoDiscoveryMechanisms 1 }


-- conformance information
ptopoConformance OBJECT IDENTIFIER ::= { ptopoMIB 4 }

ptopoCompliances OBJECT IDENTIFIER ::= { ptopoConformance 1 }
ptopoGroups      OBJECT IDENTIFIER ::= { ptopoConformance 2 }


-- compliance statements
ptopoCompliance MODULE-COMPLIANCE
   STATUS  current
    DESCRIPTION
            "The compliance statement for SNMP entities which implement
            the PTOPO MIB."
    MODULE  -- this module
        MANDATORY-GROUPS {
              ptopoDataGroup,
              ptopoGeneralGroup,
              ptopoConfigGroup,
              ptopoNotificationsGroup
        }
    ::= { ptopoCompliances 1 }

-- MIB groupings
ptopoDataGroup   OBJECT-GROUP
    OBJECTS {
         ptopoConnRemoteChassisType,
         ptopoConnRemoteChassis,
         ptopoConnRemotePortType,
         ptopoConnRemotePort,
         ptopoConnDiscAlgorithm,
         ptopoConnAgentNetAddrType,
         ptopoConnAgentNetAddr,
         ptopoConnMultiMacSASeen,
         ptopoConnMultiNetSASeen,
         ptopoConnIsStatic,
         ptopoConnLastVerifyTime,
         ptopoConnRowStatus
    }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to represent
            physical topology information for which a single agent
            provides management information.

            This group is mandatory for all implementations of the PTOPO
            MIB."
    ::= { ptopoGroups 1 }

ptopoGeneralGroup    OBJECT-GROUP
    OBJECTS {
         ptopoLastChangeTime,
         ptopoConnTabInserts,
         ptopoConnTabDeletes,
         ptopoConnTabDrops,
         ptopoConnTabAgeouts
    }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to report the
            general status of the PTOPO MIB implementation.

            This group is mandatory for all agents which implement the
            PTOPO MIB."
    ::= { ptopoGroups 2 }

ptopoConfigGroup    OBJECT-GROUP
    OBJECTS {
         ptopoConfigTrapInterval,
         ptopoConfigMaxHoldTime
    }
    STATUS  current
    DESCRIPTION
            "The collection of objects which are used to configure the
            PTOPO MIB implementation behavior.

            This group is mandatory for agents which implement the PTOPO
            MIB."
    ::= { ptopoGroups 3 }

ptopoNotificationsGroup NOTIFICATION-GROUP
    NOTIFICATIONS {
         ptopoConfigChange
    }
    STATUS        current
    DESCRIPTION
            "The collection of notifications used to indicate PTOPO MIB
            data consistency and general status information.

            This group is mandatory for agents which implement the PTOPO
            MIB."
    ::= { ptopoGroups 4 }

END

-- 
--    Copyright (C) The Internet Society (2000).  All Rights Reserved.
-- 
--    This document and translations of it may be copied and furnished to
--    others, and derivative works that comment on or otherwise explain it
--    or assist in its implementation may be prepared, copied, published
--    and distributed, in whole or in part, without restriction of any
--    kind, provided that the above copyright notice and this paragraph are
--    included on all such copies and derivative works.  However, this
--    document itself may not be modified in any way, such as by removing
--    the copyright notice or references to the Internet Society or other
--    Internet organizations, except as needed for the purpose of
--    developing Internet standards in which case the procedures for
--    copyrights defined in the Internet Standards process must be
--    followed, or as required to translate it into languages other than
--    English.
-- 
--    The limited permissions granted above are perpetual and will not be
--    revoked by the Internet Society or its successors or assigns.
-- 
--    This document and the information contained herein is provided on an
--    "AS IS" basis and THE INTERNET SOCIETY AND THE INTERNET ENGINEERING
--    TASK FORCE DISCLAIMS ALL WARRANTIES, EXPRESS OR IMPLIED, INCLUDING
--    BUT NOT LIMITED TO ANY WARRANTY THAT THE USE OF THE INFORMATION
--    HEREIN WILL NOT INFRINGE ANY RIGHTS OR ANY IMPLIED WARRANTIES OF
--    MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE.
--