RiDiag V2.1.19.0 16.03.2021

RiDiag V2.1.18.0 20.01.2021

RiDiag V2.1.17.0 19.01.2021

RiDiag V2.1.16.0 18.01.2021

RiDiag V2.1.15.0 02.12.2020

RiDiag V2.1.14.0 18.08.2020

RiDiag V2.1.13.0 18.08.2020

RiDiag V2.1.12.0 18.08.2020

RiDiag V2.1.11.0 18.08.2020

RiDiag V2.1.10.0 18.08.2020
Fixes double entry of evaporator temperature in the Live chart

RiDiag V2.1.6.0 20.02.2020
Fixes several display errors
Adds Relay Remote Control settings to chiller parameters

RiDiag V2.1.5.0 12.02.2020
Fixes display of Minichiller relay names

RiDiag V2.1.4.0 14.01.2020
Fixes #33396 - Add new Minichiller error and warning messages

RiDiag V2.1.3.0 21.11.2019
Fixes bug with onboard Realtek NIC reporting invalid USB name

RiDiag V2.1.2.0 08.11.2019
Requires Firmware 2.8.3
Adds additional variables for Minichiller Live Charts

RiDiag V2.1.1.0 06.11.2019
Fixes display of Release Notes for RiDiag software updates
Export/Import of relay configuration (for Cooling Devices)
Export/Import parameter set for Cooling Devices

RiDiag V2.1.0.0 05.11.2019
Switch release notes to English
Export/Import of relay configuration (for the Minichiller)
Export/Import parameter set for Minichiller

RiDiag V2.0.12.1
Fixes #31593 - Crash at startup when a Realtek device is connected

RiDiag V2.0.12.0 17.04.2019
Corrected display of Setpoint after writing the parameters into the device

RiDiag V2.0.11.0 16.04.2019
Restricted value range for input fields of the parameter page

RiDiag V2.0.10.0 15.04.2019
Standard view in data cockpit changed for better data overview with short uptime
Treatment of °C/°F on the parameter page
Event and error codes for chiller variants

RiDiag V2.0.9.0 08.04.2019
Logging of further device data when connecting
Unit symbol for Kelvin corrected
Automatic adjustment of the alarm threshold value in the event of changes to the setpoint value
Incorrect alarm values
Display Language is changed, but old value remains in RiDiag
Errors do not remain pending
False alarm is displayed

RiDiag V2.0.8.0 07.03.2019
Variable connection of the setpoint data point in the Minichiller flowchart corrected
Positioning of setpoint data point in Minichiller flowchart corrected

RiDiag V2.0.7.0 28.02.2019
Alarm relay configuration is not loaded correctly when first opened

RiDiag V2.0.6.0 27.02.2019
Display of flow and cooling capacity values in the device cockpit
Translation Display Color parameters

RiDiag V2.0.5.0 26.02.2019
Translation of options for alarm threshold Parameter

RiDiag V2.0.4.0 21.02.2019
Error when trying to write new data to a non-empty display is shown only once
USB driver is not automatically installed during installation

RiDiag V2.0.3.0 18.02.2019
Version information is written to the log at startup
UX Chiller Parameter Page Enhancement
Crash when calling the data cockpit in connection with display software 2.06.00

RiDiag V2.0.2.0 12.02.2019
[#18006] Live recording does not save any show/save any data (Customer license)
[#18089] Spelling error in header of page Device self-test
[#18090] Device name is displayed offset to label

RiDiag V2.0.1.0 20.11.2018
Small visual improvements

RiDiag V2.0.0.0 20.11.2018
Blue e+ Minichiller extension
USB driver included in installer
New MessageConfig bits for firmware 1.13 integrated

RiDiag V1.1.26.0 02.05.2018
Installer updated

RiDiag V1.1.25.0 17.04.2018
Corrected handling of WA number when writing on empty displays

RiDiag V1.1.24.0 12.04.2018
Handling for empty displays improved
Device instructions updated

RiDiag V1.1.23.0 21.03.2018
[#2941] Incorrect unit in CSV header for Datapoint Export
[#6655] GUI crash
[#6669] Crash at start of live recording
[#6675] v1.1.22.0 does not start any more
[#6708] Closing RiDiag leaves zombie process behind

RiDiag V1.1.21.0 07.03.2018
[#6241 ]Crash when connecting an empty display (Use case for clearing point)

RiDiag V1.1.20.0 26.02.2018
[#5939] Crash when saving the language settings

Translated with www.DeepL.com/Translator

RiDiag V1.1.0.0 23.02.2018
[#5023] Error messages for actions (where required)
[#2333] Language selection independent of operating system language
[#2683] If the service request has problems sending, display detailed error message instead of icon
[#4571] Create and restore backup files of history data
[#5025] Service Write data to device
[#5917] Allow firmware download without connected device

RiDiag V1.0.59.1 16.08.2017
[#8179] Device Cockpit with Customer Level License not available

RiDiag V1.0.58.1 25.07.2017
Logfiles keep the extension .log when rotating.
[#8098] Crash when booting on Windows 10 Laptop
[#7384] Missing field restriction for license entry
made the label of the checkbox clickable
[#8092] Missing "Trim" commands for license fields

RiDiag V1.0.57.0 10.07.2017
Version adapted for development release

RiDiag V1.0.56.0 06.07.2017
[#8047] System messages are not available at LicenseLevel.None
log4net updated to version 2.0.8

RiDiag V1.0.55.0 15.05.2017
[#7860] English manual missing
Application started without Language File again in system language
Improved version handling when downloading software updates

RiDiag V1.0.53.0 09.05.2017
[#7144] email of a spare parts request will not be sent

RiDiag V1.0.48.0 28.03.2017
[#6805] Long-term measurement -> follows a crash
[#7129] Ridiag started ->Logged on after a long time -> Ridiag crashes
[#7257] Crash after standby operation
- The switchover to standby/hibernate mode is delayed so that the port can be closed correctly.
  RESTRICTION: It may still not be possible to connect to the RACC after the resume.
                 Then the USB connection must be disconnected briefly and RiDiag restarted (USB driver problem).

RiDiag V1.0.47.0 21.03.2017
[#5992] RiDiag Update - Release Notes are hidden - Update only works if a new valid version is stored in Cumulus 
Help with revision number
Project references corrected 
Better logging of unhandled exceptions 
Return of a boolean if the license check result is negative, instead of handing over the exception. 
Project references corrected 
[#7241] RiDiag crash during connection setup 
Incorrect change undone. 
ReconnectButton now actually allows a reconnect in case the connection has r613
Description corrected for self-test. 
Documentation updated - version 2017-02-20

RiDiag V1.0.46.0 01.02.2017
Create folder for license file if not available
Create folder for settings file if not available
[#7192] offline Configuration->Analysis ->Data Cockpit-> crash follows
[#7105] after upgrade ->Analysis ->Data Cockpit ->follows Crash

RiDiag V1.0.45.0 24.01.2017
Change to the installer. The folder RiDiag in C:\ProgramData\Rittal must be deleted before installation.
Setting IsOfflineData after deserialization
Device off USB - Show connection only if ArticelNumber is ok
[#7123] changed to 'Fahrenheit ->Live recording values in .csv file are in °C
Export to set instrument unit (°C °F)
[#7160] Crash occurs after pressing the Flash button
 -> general adjustment of file save (set extended rights for everyone)
[#7168] Application Crash
[#7166] USB connection
Updated help texts
Updated language files

RiDiag V1.0.44.0 09.01.2017
[#7130] Analysis-> Data Cockpit-> Crash
[#7131] Device->Configuration->Reset factory settings->USB icon in upper menu bar changes to Oflline icon
English help added, German help updated.

RiDiag V1.0.43.0 19.12.2016
[#6563] Navigate in the main menu during the charging process-> a crash occurs 
[#6805] Long-term measurement -> follows a crash
[#6897] after another device is connected the update is not complete
[#7037] RiDiag Crash
[#7039] Live recording only takes on an evaporation temperature 
[#7082] Wrong error is displayed
[#7101] Connect with Blue e+ ->click on Home Button->Connection no longer displayable
[#7115] The factory setting selection causes a crash.
[#7106] Help->Notes Heading missing
[#7105] after upgrade ->Analysis ->Data Cockpit ->follows Crash
[#7104] Firmware Update ->Button in lower area Finished and Reports not yet available
[#7100] Analysis -> Data Cockpit ->follows Crash

RiDiag V1.0.42.0 07.12.2016
German help built in
Connection changed --> hopefully no longer crashes because of usb problems.
Storage time and RiDiagVersion is displayed for offline datasets.
B6 if error also in FlowChart Magenta
t? --> tex flowChart
[#6904] local data set ->Analysis ->Long-term measurement to be grayed out
[#7040] Offline project engineering
[#7012] Help->Notes not yet available and 
[#7011] Settings->Privacy->Header missing

RiDiag V1.0.41.0 28.11.2016
[#6911]
[#6910]
[#6909]
[#6908]
[#6906]
[#6904]
[#6888] Equipment Cockpit->After conversion to Farenheit the values remain in Celsius

RiDiag V1.0.40.0 18.11.2016
License built into the installer
Functional scope free , customer , service added
Icons exchanged in FlowChart.
Print button removed from data cockpit

RiDiag V1.0.39.0 16.11.2016
[#6886] for total cooling capacity and operating voltage Entries not yet available
[#6893] device->spare part inquiry ->spare part table is no longer available
Fixed [#6903] When selecting spare parts the text turns black
View SEER in DataCockpit
Licence and data protection texts in english
Save button inactive if local data
language files updated
[#6889] After switching from F° to C° ->Update -> the values remain in F° 
[#6888] Equipment Cockpit->After conversion to Farenheit the values remain in Celsius
[#6887] Cockpit efficiency at Fahrenheit wrong values

RiDiag V1.0.38.0 14.11.2016
Bugfix: Ignore duplicate timestamps in CSV history file. Last line for the same timestamp will be taken over.
first try to fix [#6897] after connecting another device the update is not complete
RPF references updated.

RiDiag V1.0.37.0 09.11.2016
Fixed bug with longtermmeasurement
fixed bug with transfer of relay configuration
remove network icon on start page
remove filtermat changed date
PrivacyNotice and LicenseAgreement added.
[#6874] English language: Settings->License conditions->Crash
[#6883] Startscreen Devices Selection->Click USB Button->Connect->Click House Icon->Crash
[#6885] From the menu bar 'Network' and 'Component Runtime' should be hidden.

RiDiag V1.0.36.0 03.11.2016
initial