Liquid cooling packages
-
Liquid Cooling Package LCP rack DX, LCP rack DX/FC
Rack-based cooling on one to two IT racks. Continuous cooling output adjustment due to the use of an output-controlled compressor in the LCP Rack DX (evaporator) An external condenser is required to operate the unit.
-
Liquid Cooling Package LCP Inline DX, LCP Inline DX/FC
Ideal for cooling of small and medium-sized IT applications.
-
Liquid Cooling Package LCP Hybrid CW
Large-scale, high-capacity air/water heat exchanger, designed as the rear door of the server enclosure, ensures that heated waste air from the servers is cooled down to server intake air level.
-
Liquid Cooling Package LCP Rack CW, LCP Rack CWG
Cooling via high-performance compact impellers. The LCP draws in the air at the sides at the rear of the server enclosures and blows the cooled air back into the front part of the server enclosure at the sides.
-
Liquid Cooling Package LCP Inline CW, LCP Inline CWG
Bayed climate control designed for siting within a bayed enclosure suite. The hot air is extracted at the rear of the unit, cooled and then expelled forwards to the cold aisle.