Press releases

Rittal: Lefdal Mine Datacenter is open

15.05.2017. Being the most cost effective, secure, flexible, and green datacenter in Europe – that is the vision of Lefdal Mine Datacenter (LMD) in Norway. Opened on 10th May 2017, the datacenter has completed the build out of Phase 1, and a cooling capacity of 45 MW is ready for use.

Read article!
  • Slimline motor controllers create space in enclosures

    23.01.2018. Small drives for machines and equipment often lie in the range of up to 9.0 A and are protected by conventional motor circuit breakers. With the new motor controllers for its RiLine Compact power distribution system, Rittal is now able to offer a sophisticated solution using new technology that is far from ordinary.

  • Kiesling wins Supplier Special Award

    18.01.2018. Rittal subsidiary Kiesling Maschinentechnik GmbH & Co. KG in Wiernsheim has received the Supplier Special Award from the Maag Group in Grossostheim as one of its top three suppliers.

  • Youngsters cracked it

    11.12.2017. After three months spent polishing their projects, the best efforts by the second-year apprentices in the Friedhelm Loh Group earned special prizes. During this year’s summer workshop in Gnadenthal Abbey, the youngsters focused on the principle “You have to crack open a nut to see what’s inside”.

  • The new "be top" company magazine: The pacemaker

    07.12.2017. Time flies – and nowhere is this more true than in today’s digitised world. This makes smooth processes and reliable partners all the more crucial. The new edition of be top shows why Rittal considers itself a pacemaker for industry and IT when it comes to supporting partners on their paths to success.

  • Rittal at SPS: Rittal expands RiLine Compact portfolio

    30.11.2017. Small drives for machines and equipment often lie in the range of up to 9.0 A and are protected by conventional motor circuit breakers. However, when space in the enclosure is limited, it is very difficult to accommodate a high number of protection elements.

  • Rittal at SPS: New height-adjustable support section from Rittal

    29.11.2017. Optimised ergonomics are essential in the work-place. Not only do machines need to satisfy safety requirements, but they must also be designed so that they are as easy to use as possible, i.e. effortless and strain-free. Operator terminals on machines should be flexible and easy to position, using support arm systems.

  • Andreas Huck new Chief Financial Officer of the Friedhelm Loh Group

    06.11.2017. The operational divisions of the Friedhelm Loh Group have a new head of finance and administration: Andreas Huck has been Managing Director within the Group since 1st September 2017. He takes over the management of the Finance and Administration division at Rittal and is also responsible of Loh Services.