Cart

Rittal - Press releases - The global leader of Weatherproof Boxes and Industrial Electrical Enclosures

International partnership offers great marketing platform

2014-03-12. Rittal entered a worldwide partnership agreement with DatacenterDynamics (DCD), London, in the field of marketing. As a result, the provider of IT infrastructure has been granted international access to the services of DatacenterDynamics, allowing Rittal to present its data centre portfolio to a larger audience.

Read article!
  • Enhanced for extreme applications

    2019-02-14. The new Rittal VX25 large enclosure system delivers significantly enhanced value to electrical engineering companies thanks to its technical features, ease of assembly and high levels of safety.

  • Rapid assembly for secure distribution

    2019-01-30. Rittal has developed four compact PDU (Power Distribution Units) systems for professional power distribution in IT racks which will halve the time a system takes to assemble, compared to screw-in PDUs.

  • Outstanding Cooling From Above

    2019-01-29. Rittal has developed a roof-mounted version of its award-winning and highly energy efficient Blue e+ cooling units; these are designed for enclosures of 800 x 600mm (W x D) upwards and deliver a cooling output of 1.3 kW.

  • Five Trends for Cloud Computing and Data Centres

    2019-01-23. Rittal has issued predictions for the data centre sector as the industry moves towards greater AI-based monitoring capabilities and the processing of data in real time with edge computing.

  • Bright Ideas from Rittal

    2019-01-03. If your data centre is in need of better illumination, then Rittal can help. The company will be offering enlightenment at its Stand D610 at Data Centre World, London, from 12-13 March 2019.

  • Dancing Robots are a reality at Rittal’s Manufacturing Plant in Germany

    2018-11-20. High-tech production plants that “think for themselves”, that plan things automatically and that optimise maintenance work through artificial intelligence, might sound like a futuristic sci-fi film, but it is fast becoming a reality at Rittal’s manufacturing plant in Rittershausen, Germany.