C Rails
-
C rails 30/15 to EN 60 715 for VX, TS, VX SE
Mounted directly on the horizontal enclosure profile or base configuration rail for TP, on the vertical enclosure profile using additional fastening components.
-
C Rails for TS, VX SE
For direct external mounting between the vertical TS, SE enclosure sections. The C-section angle bracket is additionally required for mounting between the horizontal TS, SE enclosure sections. Because the attachment piece is designed for universal use, the C rails may optionally be attached to the inner or outer level of the TS 8 frame.