Accessories to improve handling
-
Installation kit for back-to-back mounting plates
The minimum spacing between the mounting plates facilitates maximum assemblies on both mounting plates.
-
Cross-brace for mounting plates for VX, TS, SE
Additional horizontal rigidity for vibration damping and/or retrospective stabilisation of wide mounting plates. This brace may also be used as an attachment aid for heavy components.
-
Partial mounting plate holder for partial mounting plate VX
The partial mounting plate may be fitted set back by 20 mm behind the enclosure frame using the partial mounting plate holder, and also fastened to the frame from the outside. The partial mounting plate is also removable from the inside for servicing.
-
Hinge attachment for partial mounting plate VX
In conjunction with the mounting kit for swing frames, small, the partial mounting plate can be hinged to allow access to the components behind it for servicing.
-
Installation kit for mounting plates TS, SE, back-to-back
The minimal distance between the two mounting plates ensures a maximum installation depth for installed equipment on both sides.
-
Mounting plate infill for VX, TS
For a continuous mounting surface in bayed suites where the mounting plate is set forward.
-
Transport handle for mounting plates for VX, TS, SE
May be used at any given position in the side C-fold
-
Mounting plate adjustment bracket for KS
Infinitely adjustable. Other equipment can also be installed on a rail system, instead of the mounting plate.
-
Hinge attachment for partial mounting plate TS, SE
For vertically hinged attachment of partial mounting plates.
-
Support rail, locatable for TS, CM, PC, TP
To accommodate mounting plate, small, if due to mounting plate infill or similar equipment, vertical no punched sections or other assemblies can be mounted in the depth.