The Complete Guide to Direct Liquid Cooling for AI Data Centers

November 10 2026

Technical Insights

AI training racks in Indian data centers can move from conventional 5–10 kW rack loads to 40–140+ kW per rack, depending on GPU configuration. In summer conditions above 35–40°C, monsoon humidity, and constrained white space capacity, direct liquid cooling for AI data centers becomes a practical thermal design option rather than an experimental upgrade.

Rittal supports this shift through modular IT cooling architectures for high-density racks, including liquid-to-air and liquid-to-liquid approaches. This guide explains how direct liquid cooling works, where it fits, and what Indian data center teams should evaluate before deployment.
 

Why AI Data Centers Need Advanced Cooling Solutions

AI training and inference concentrate heat at GPUs, CPUs, and accelerators. As rack power rises towards 40–140+ kW, air cooling can lose headroom, increasing thermal throttling risk, fan energy, and operating cost.

What Is Direct Liquid Cooling in AI Data Centers?

Direct liquid cooling is a thermal management method where heat is transferred to a liquid at or very near the heat source instead of first being rejected into room air. The US Department of Energy describes this as moving waste heat to liquid close to the component. In AI infrastructure, cold plates are fixed to high-power components such as GPUs and CPUs. A coolant loop then carries heat away to a coolant distribution unit, heat exchanger, or facility cooling system.

ASHRAE, the American Society of Heating, Refrigerating and Air-Conditioning Engineers, defines direct water-cooled servers as systems where heat is transferred to an attached heat-transfer component such as a cold plate. For engineers evaluating liquid cooling for AI data centers, this definition separates direct-to-chip systems from room-level air cooling.
 

How Direct-to-Chip Liquid Cooling Works

Direct-to-chip cooling removes heat from processors through a controlled liquid loop. A typical process follows these steps:

  1. Cold plates are attached to GPUs, CPUs, or other high-heat packages. Confirm mechanical compatibility with the server platform before procurement.
  2. Coolant absorbs chip heat through the cold plate surface. Specify coolant chemistry and material compatibility before installation.
  3. A pump circulates liquid through manifolds and hoses. Verify flow rate, pressure drop, and redundancy requirements during design review.
  4. A CDU cooling system transfers heat between the IT loop and the facility loop. Select CDU capacity based on rack power and allowable supply temperature.
  5. The facility cooling system rejects heat through chilled-water systems, dry coolers, or cooling towers, with heat-rejection capacity modulated to maintain reliable operation under peak Indian summer conditions.

Direct-to-chip cooling has become common in AI and high-performance computing because it can typically capture 70–90% of server heat in liquid, depending on server design. Remaining heat from memory, voltage regulators, and storage still requires air-side management.
 

Key Components of a Direct Liquid Cooling System

A complete data center liquid cooling design depends on the server interface, distribution equipment, pumps, and facility heat rejection path. The engineering task is to maintain stable chip temperatures without introducing leakage, water quality, or serviceability risks.

Cold Plates

Cold plates are metal heat exchangers attached directly to GPU and CPU packages. They capture heat at the component surface and transfer it into a secondary coolant loop. For high-power AI nodes, cold plate design affects thermal resistance, pressure drop, and maintainability. Check server vendor specifications before finalizing rack and manifold design.

Coolant Distribution Unit (CDU)

A coolant distribution unit, or CDU, manages coolant flow, temperature control, pressure, and separation between the IT cooling loop and the building water loop. It is the central control point for direct-to-chip deployments.

Rittal offers liquid-to-liquid CDU options for high-density AI racks, including in-rack and in-row architectures with cooling outputs ranging from around 150 kW per rack to up to 1 MW per system, depending on configuration. Use these figures as planning references and verify the current specification for the selected model.
 

Pumps and Cooling Loops

A primary loop usually connects the CDU to the facility cooling system. A secondary loop supplies controlled coolant to server cold plates and rack manifolds. This separation helps protect IT equipment from facility water quality variation. For Indian sites, specify filtration, conductivity limits, glycol concentration where required, and leak detection points during commissioning.
 

Benefits of Direct Liquid Cooling for AI Data Centers

The main benefit is not only lower chip temperature. It is the ability to operate dense AI infrastructure with predictable thermal performance and a lower dependence on high-volume air movement.

Supports High-Density AI Hardware

Dense GPU clusters create rack loads that may exceed the practical limits of conventional air cooling. High-density data center cooling using direct-to-chip loops can support 50–140+ kW per rack in suitable designs, depending on server and facility conditions. This helps data center managers plan AI zones without over-expanding white space. Procurement teams should still confirm rack weight, power distribution, and manifold compatibility.

Improves Energy Efficiency

Air-cooled AI servers rely heavily on fans and low supply-air temperatures. Liquid can carry more heat per unit volume than air, so direct-to-chip systems can reduce air-side cooling demand. ASHRAE water classes W2 and W3 allow building-supplied water temperatures from 17.2°C to 32°C and up to 43°C, respectively. This can improve energy efficiency where dry coolers, cooling towers, or warmer water loops are viable.

Increases Hardware Reliability

Unstable chip temperature can cause thermal throttling, reduced performance, or premature component stress. Liquid cooling helps maintain tighter thermal control near the processor package. For operators, the practical reliability gain depends on correct commissioning. Monitor flow, temperature, pressure, and leak alarms continuously rather than treating the cooling loop as passive infrastructure.

Direct Liquid Cooling Challenges for Indian Data Centers

Indian deployment requires site-level checks, not only rack-level cooling calculations. Climate, water strategy, and maintenance capability can decide whether the architecture performs as intended. Summer ambient temperatures in Delhi-NCR, Hyderabad, Chennai, and Mumbai can exceed 35–45°C. Design the heat rejection system for peak conditions, not only annual averages.

Water availability varies significantly by region. Where cooling towers are restricted or water quality is poor, evaluate dry coolers, closed loops, and treatment requirements. Existing facilities may not have pipe routes, raised-floor capacity, or rack layouts suitable for manifolds. Survey the white space and plant room before ordering server clusters.

Skilled maintenance is also essential. Train operations teams on coolant sampling, quick disconnects, leak response, and CDU alarms before live workload migration. The initial deployment cost can be higher because CDUs, manifolds, cold plates, and facility integration are required. Compare capital cost with lifecycle energy, rack density, and avoided expansion costs in INR.
 

Implementing Direct Liquid Cooling in Data Centers

Implementation should begin with measured load data, not assumptions. Treat direct liquid cooling as a mechanical, electrical, and IT integration project.

Evaluate Existing Infrastructure

Review rack power, UPS capacity, floor loading, pipe routes, air containment, and current cooling headroom. AI planners may need to assume 30–60 kW per rack for mid-range GPU nodes and 80–140 kW per rack for leading liquid-cooled platforms.

Action: create a rack-by-rack capacity schedule covering power, cooling, structural load, and service clearance.

Select Suitable Cooling Architecture

Direct-to-chip cooling suits many AI and HPC deployments because it keeps servers in standard rack formats while capturing most processor heat in liquid. Immersion cooling submerges hardware in dielectric fluid and can support very high densities, but it requires different service practices.

Hybrid approaches combine direct-to-chip cooling with rear-door heat exchangers or air cooling for residual heat. Action: select the architecture after comparing workload density, server warranty conditions, facility water readiness, and maintenance capability.

Plan Maintenance and Monitoring

A reliable system needs leak detection, coolant quality checks, pump monitoring, temperature sensors, and alarm integration with building management systems. The CDU should provide visibility into flow and temperature deviations.

Action: define operating limits, sampling intervals, alarm escalation, and spares before the first production workload is commissioned.

Future of Direct Liquid Cooling in India’s AI Data Center Market

AI adoption, cloud computing, and high-performance computing are increasing the need for scalable thermal zones in India. ASHRAE’s AI data center framework recommends liquid or liquid-assisted architectures for 50–140+ kW racks while maintaining energy and thermal efficiency goals.

Future Indian AI facilities are likely to combine air, rear-door heat exchange, direct-to-chip, and liquid-to-liquid CDU systems. The deciding factors will be the required rack density, site climate, water strategy, and lifecycle operating cost.

Conclusion

The core takeaway is that direct liquid cooling is most relevant when AI rack density exceeds the practical limits of air cooling and the site can support disciplined fluid management. Before specifying equipment, you should verify rack power, facility heat rejection, coolant quality, leak detection, and maintenance readiness under Indian ambient and humidity conditions. Rittal’s liquid cooling capabilities, together with planning tools such as CDU Data Center design configurators, can support an engineering review without forcing a single architecture too early.

FAQs About Direct Liquid Cooling for AI Data Centers

It transfers heat from GPUs and CPUs to coolant through cold plates, then rejects that heat through a CDU and facility cooling loop.
 

Liquid cooling removes heat from a point closer to the chip and can support higher rack densities than air cooling, depending on server and facility design.
 

It can have a higher initial cost due to CDUs, manifolds, cold plates, and piping, but lifecycle economics may improve at high rack densities.
 

Yes, some facilities can be upgraded in phases, but teams must check rack layout, pipe routes, power capacity, leak detection, and heat rejection.
 

Direct-to-chip uses cold plates on components. Immersion cooling submerges IT hardware in dielectric fluid and requires different service practices.