Rittal cooling units

Cool when the heat is on

Soltau is something of a hotspot. When the ovens at Harry-Brot reach over 200 degrees Celsius, the bread rolls and loaves aren’t alone in feeling the heat. The company’s staff and equipment also work up a sweat. Despite a room air temperature of 45 degrees, everything needs to run like clockwork – excellent test conditions for the new Blue e+ cooling units from Rittal.

Overview

Project
New Blue e+ S cooling devices at Harry-Brot
Location
Soltau, Germany
Branch
Food-and-Beverage-Industry
Challenge

Continuous operation in bakery at high temperatures

Heat-related breakdowns

High temperatures inside enclosures

 

Solution

Test of new Rittal Blue e+ S cooling unit in hot environment

Comparison with Blue e+ device in order to get reliable results

More than 60% savings with Blue e+ S device

No breakdowns any more

 

 

Wonderful aroma of bread fills the air. Every day, the ovens at Harry-Brot in Soltau turn out products including some 180,000 sandwich loaves. Freshly baked, they make their way through the production section and are then packaged and loaded into lorries to embark on their journey to supermarkets across Germany. The country’s biggest manufacturer of bakery products is a household name, with a range that includes everything from brown and wholemeal bread to sliced loaves for making toast and sandwiches.

To ensure everything goes like clockwork, systems need to be in continuous operation. It hasn’t always been that way, however. Heat-related breakdowns used to be a regular occurrence at the plant. These were mainly caused by the failure of control technology installed in enclosures, and the consequences were huge. “When our systems go down, it also brings our lorries to a standstill, and we are unable to deliver our bread. That’s a big problem, because our customers expect to find fresh bread on the supermarket shelves every day,” explains Björn von Frieling, the site’s Workshop Manager.

Bread dough moving along a conveyor belt. If systems go down, this also brings the lorries to a standstill, and no bread can be delivered.

Even though temperatures outside the enclosure can often reach 45 degrees, temperatures inside are much, much higher. They have been measured at between 60 and 70 degrees in the past – hardly the ideal conditions for sensitive electronics, especially when installed in relatively small compact enclosures. Rather than climate control units, Harry-Brot had simply been using fan-and-filter units for these enclosures. The reason for this was simple. “Cutting-edge, energy- efficient Blue e+ cooling units from Rittal were previously only available with high cooling outputs of at least 1.6 kW – definitely too high for our purposes,” explains von Frieling.

He was therefore delighted when Rittal launched the new Blue e+ S-units with lower cooling outputs. “These are ideal for the levels of heat generated by our application. In consultation with the Rittal sales team, we agreed on a trial here at the plant to put the units through their paces in our operation,” he says.

SURPRISING TEST RESULT

Besides ensuring high system availability, Harry-Brot also considers reducing the company’s carbon footprint to be a top priority and therefore prefers to invest in energy-efficient technologies. Accordingly, it used the trial to compare a new energy-efficient Blue e+ S cooling unit with a Blue e unit that had also previously been available with a lower cooling output. For both units (500 W), the energy consumption was measured continuously during the trial.

The result for the first five months surprised von Frieling. “I wouldn’t have expected a result like that,” he reveals. The Blue e+ unit consumed just 248 kWh of electrical energy, compared with 626 kWh for the Blue e unit. This corresponds to savings of 60 per cent over the entire test period and 884 kWh for the year as a whole.

Based on an average industrial electricity price of around 26 cents per kilowatt-hour, Harry-Brot can thus achieve an annual saving of around 230 euros per cooling unit. What’s more, Blue e+ units come with integrated condensate evaporation. Excluding the proportion of energy consumption accounted for by this function, the saving is over 260 euros per cooling unit.

BREAKDOWNS SOON A THING OF THE PAST

Even more important for von Frieling, though, is the higher availability that can be achieved with enclosure climate control. Effective climate control in enclosures means production systems break down less often. “That will make it easier for us to guarantee the delivery of fresh bread,” he insists. Production stoppages due to excessive enclosure temperatures are also bad for sustainability.

Components need to be replaced or repaired, which requires manpower and materials. The new enclosure climate control system will ultimately mean these resources are not called upon. Dozens of enclosures at Harry-Brot are therefore set to be equipped with Blue e+ S cooling units in the near future.

FURTHER REDUCTION IN ENERGY CONSUMPTION

The high energy efficiency of enclosure climate control is contributing to a long-term corporate strategy that has already been initiated for the entire production operation. Between 1999 and 2018, the energy consumption per metric ton of flour fell from around 1200 kWh to just over 800 kWh.

The Blue e+ S units are helping reduce this figure further. As a result, von Frieling can imagine the system also being used at other company sites in the future.

Read the full story

Contact Us