Data Centers in India: Power, Cooling, Racks and Future-Ready Design

August 11 2026

Data Centers in India: Power, Cooling, Racks and Future-Ready Design

India's digital economy is expanding faster than the infrastructure built to support it.

India's digital economy is expanding faster than the infrastructure built to support it. Cloud adoption, data localisation rules, and rapid AI rollout mean data centers in India are being commissioned across Mumbai, Chennai, Hyderabad, and a growing list of Tier-2 cities. Behind each facility sits a set of interlocking decisions: how power is supplied and backed up, how heat is removed, how racks are sized, and how the system scales, all with Indian site conditions in view.

What Is a Data Center and Why Does Its Design Matter?

A data centre is a purpose-built facility housing the servers, storage, and networking equipment an organisation depends on to run applications and store data. What separates a well-designed facility from a liability is how its power, cooling, and rack systems work together under load to ensure the uptime of the Data center.

Reliability, Scalability and Energy Efficiency

Reliability determines whether a facility stays online through a grid outage or hardware fault, usually expressed through redundancy levels rather than a single number. Scalability determines whether it can absorb a jump in rack density, say from 6kW to 30kW, without a redesign. Energy efficiency ties both together, an area Rittal has focused much of its engineering on, from cooling unit design to rack-level power distribution.

Power Infrastructure and Redundancy in Data Centers

Utility Supply, UPS Systems and Backup Generators

Most Indian facilities draw a primary feed from the state utility grid, stepped down through dedicated transformers to IT-equipment voltages. Between an outage and generator start-up, uninterruptible power supply (UPS) units bridge the gap, typically providing five to ten minutes of battery autonomy. Diesel generators remain the standard backup source for data centers across India, sized to cover the full IT and cooling load.

Understanding N, N+1 and 2N Redundancy

Redundancy describes spare capacity carried beyond normal demand. N is the baseline, with no built-in backup; N+1 adds one extra unit, such as a UPS module or cooling unit, so a single failure does not interrupt operations; 2N duplicates the entire path end-to-end into two independent systems. Most enterprise-grade data centers in India target N+1 at minimum, while BFSI and government workloads increasingly specify 2N.

Data Center Cooling Systems in India

CRAC, CRAH and Chilled-Water Cooling

Computer room air conditioners (CRAC) use a built-in compressor and refrigerant loop to cool air locally, while computer room air handlers (CRAH) rely on chilled water from a separate chiller plant. Chilled-water systems scale more efficiently at larger capacities; CRAC units suit smaller, standalone rooms. Rittal's data center cooling systems are designed from room-level units to rack-level climate control.

Hot-Aisle and Cold-Aisle Containment

Arranging racks so intake fronts face each other in a cold aisle, with exhausts venting into a shared hot aisle, stops warm exhaust air recirculating into equipment intakes. Physical containment, whether curtains, doors, or ceiling panels, seals that separation or avoids air short cycling and can meaningfully cut cooling energy use. For most Indian facilities running mixed rack densities, it is now standard practice.

InRack – InRow Cooling for High Performance computing

  • The "Front-to-Back" Principle: Hot air is drawn from the rear, passed through high-capacity heat exchangers, and delivered as cooled air directly to the 482.6 mm (19") server level.
  • InRack & InRow Closed Loop Cooling: Data centre cooling systems are engineered for optimal performance, utilizing closed loop architectures for both Direct Expansion (DX) and Chilled Water (CW) configurations. By isolating rack or row-level thermal loads from the broader room environment, these solutions enable precise heat removal directly at the source. Because the system operates independently of ambient room air-conditioning, it effectively eliminates hot spots and maintains stable, high-efficiency conditions for sensitive ICT equipment.
  • EC Motor Efficiency: Utilizing Electrically Commutated (EC) fans, the LCP offers linear speed control from 0% to 100%. This allows the system to adapt instantaneously to actual volumetric flow requirements, drastically reducing electrical consumption compared to traditional AC motors.
  • Intelligent Ecosystems: Every Cooling unit is backed by sophisticated monitoring software, providing preventative analysis and real-time visualization of fan speeds and thermal gradients to ensure zero service-related downtime.

Liquid Cooling for AI and High-Density Computing

Air cooling struggles once rack loads climb past roughly 20-50kW, a threshold AI training and HPC racks now regularly exceed. Liquid cooling circulates coolant media or a dielectric coolant close to, or directly onto the coldplates , the heat-generating Graphics processors unit (GPU), since water carries far more heat than air. Rear-door heat exchangers and direct-to-chip cold plates are the two most common approaches, and modular liquid cooling packages now handle loads of up to 50kW~140 kW or even more per enclosure. Rittal's CDU In-Row liquid-to-liquid coolant distribution unit for high-performance servers.

Server Racks and White-Space Design

The rack is where power, cooling, and IT hardware physically meet, so data center rack design decisions ripple through every other system.

Choosing Rack Size, Depth and Load Capacity

The 19-inch rack is the global standard for server racks for data centers, measured in rack units (1U = 44.45mm), with heights commonly running 24U to 47U. Standard outer widths are 600mm or 800mm, with depths of 1,000mm to 1,200mm for modern servers and cable clearance. Load capacity ranges from around 750kg for low-density racks to over 1,500kg for high-density ones; check floor load certification on upper floors of Indian multi-tenant buildings.

Planning Rack Density and Power per Rack

Rack density, in kW per rack, should be planned around the actual hardware roadmap rather than a facility-wide average, since one high-density row can undermine a cooling design sized for the mean. Legacy enterprise racks in India commonly run 3-6kW, virtualised workloads 8-15kW, and AI or HPC racks 30kW and climbing. Intelligent PDUs with real-time metering help track draw per rack and catch imbalances early.

Airflow, Cable Management and Temperature Monitoring

Blanking panels over unused rack space stop cold air bypassing equipment, a low-cost fix that measurably improves cooling efficiency. Structured cable management keeps airflow paths clear and simplifies fault-finding. Temperature sensors at server inlets, tied into monitoring platforms such as CMC III, give early warning of hotspots and automatically opening door in case of emergency for CMC III ADO.

Sustainable and Future-Ready Data Center Design

PUE, WUE and Renewable Energy

Power Usage Effectiveness (PUE), the ratio of total facility power to power consumed by IT equipment, is the standard efficiency benchmark; 1.0 is the theoretical ideal, and new Indian builds increasingly target figures well below the 1.5-1.6 many older facilities still run. Water Usage Effectiveness (WUE) matters just as much in water-stressed Indian cities, since evaporative cooling can consume volumes of water that dry or hybrid systems avoid. Renewable power purchase agreements, particularly solar and wind contracts in states such as Gujarat and Tamil Nadu, are becoming standard for new capacity.

Preparing for AI and Higher Rack Power Densities

AI workloads are pushing rack densities well beyond what most existing Indian facilities were designed for, with some hyperscale deployments now planning for over 50kW per rack. Retrofitting an air-cooled facility for that load is expensive, so forward-looking designs build in liquid-ready busbars, reinforced floor loading, and cooling headroom before demand requires it.

Modular Infrastructure and Scalable Capacity

Modular construction, using pre-fabricated power, cooling, and rack modules that connect at standardised interfaces, lets operators add capacity in defined increments rather than over-building. Container-based designs can be deployed in weeks rather than months, suiting compressed Indian expansion timelines.

How to Choose a Data Center Infrastructure Partner

Evaluating data center providers comes down to a few questions. Can they support power, cooling, racks, and monitoring as one coordinated system rather than separately sourced components? Do their products carry certifications relevant to Indian conditions, and can local service keep downtime to a minimum? Rittal, for instance, pairs its rack, power, and climate control portfolio with simulation tools such as RiTherm, IT Cooling calculator & Computational Fluid Dynamics Software CFD simulation to model thermal performance before installation.

Frequently Asked Questions About Data Centers in India

A data centre's core components are power supply with UPS backup, cooling systems, server racks, structured cabling, fire suppression, and monitoring software.

Rack power demand ranges from 5-10kW in legacy setups to 50kW~140 kW or even more for AI and HPC workloads, depending on cooling design and redundancy.

Chilled-water with closed loop cooling which means cooling near to IT equipment’s with solid or glass doors for Racks and hot/cold aisle containment suit most Indian facilities; liquid cooling is best for high-density AI racks above 50kW.

The industry standard is a 19-inch rack, usually 42U tall, with 600mm or 800mm widths and depths of 1,000mm to 1,200mm. Also the OCP Racks which supports the housing of high-performance servers or GPU servers comes with 21 inch Rack, usually 44OU.

Not always, but it becomes necessary once rack densities pass roughly 40-50kW, a threshold many AI and HPC deployments now exceed, moreover the HPC should support the liquid cooled connections