Understanding IP Ratings in Ex Enclosures and How They Impact Your Safety

December 17 2025

Understanding IP Ratings in Ex Enclosures and How They Impact Your Safety

Safety in hazardous industrial environments, such as oil and gas plants, chemical processing facilities, refineries, mining operations, and pharmaceutical facilities, is critical due to the presence of explosive atmospheres.

Introduction

Safety in hazardous industrial environments, such as oil and gas plants, chemical processing facilities, refineries, mining operations, and pharmaceutical facilities, is critical due to the presence of explosive atmospheres. Ex enclosures, also known as explosion-proof enclosures, play a vital role in protecting sensitive electrical equipment within these dangerous zones. While their primary role is to contain internal explosions, another equally important function involves protecting internal components from external environmental factors such as dust, dirt, and moisture.

This is where IP ratings (Ingress Protection ratings) become essential in understanding how well an Ex enclosure can safeguard equipment and ensure safety. This blog explores the meaning of IP ratings, their composition, and their crucial impact on safety and equipment protection in hazardous environments, with a focus on Ex enclosures.

What is an IP Rating?

An IP Rating is a standardized code developed by the International Electrotechnical Commission (IEC) under IEC 60529:1989 (also known as EN 60529), which classifies how well an enclosure protects against intrusion by solid objects (including dust and fingers) and liquids such as water.

The IP code consists of the letters "IP" followed by two digits. Each digit indicates a different type of protection:

  • First digit: Protection against solids (dust, dirt, tools, etc.).
  • Second digit: Protection against liquids (water, moisture, spray, immersion).

If a digit is replaced by an “X” (e.g., IPX7), it means the equipment has not been tested or rated for that type of protection.

Unlike vague terms such as “waterproof” or “dustproof,” IP ratings provide precise, measurable levels of protection, essential for engineers, safety managers, and end users.1

Why IP Ratings Matter in Ex Enclosures

Ex or Increased Safety enclosures primarily contain internal explosions to prevent ignition of explosive atmospheres. However, dust and moisture ingress can cause electrical faults, triggering sparks or overheating that might lead to dangerous external ignition.

Thus, robust IP-rated sealing is critical to:

  • Maintain the integrity and safety of internal electrical systems.
  • Prevent dust accumulation and moisture ingress that could lead to failure or ignition.
  • Ensure compliance with safety regulations and standards in hazardous zones. 

In summary, IP ratings provide a critical secondary layer of protection for Ex enclosures, supporting their explosion containment function throughout their operational life.

Understanding IP Ratings in Ex Enclosures

The Two Digits of an IP Rating

An IP rating, e.g., IP66, comprises:

  • First digit (0-6): Solids protection, ranging from no protection (0) to complete dust-tightness (6).
  • Second digit (0-9K): Liquids protection, from no protection (0) to protection against high-pressure, high-temperature water jets (9K).1
     

First Digit: Protection Against Solids

DigitProtection LevelDescription
0No protection-
1Protection against large objects>50 mm diameter (e.g., hand)
2Protection against fingers>12.5 mm diameter
3Protection against tools & wires>2.5 mm diameter
4Protection against most wires>1 mm diameter
5Dust-protectedDust ingress is limited but safe for operation
6Dust-tightNo dust ingress; complete protection

 

High dust protection (IP5X or IP6X) is essential in hazardous zones dealing with explosive dust and particulates.

Second Digit: Protection Against Liquids

DigitProtection LevelDescription
0No liquid protection-
1Protection against drippingVertically falling drops
2Protection against tilted drippingFalling drops up to 15° tilt
3Protection against spraysSpray up to 60° from vertical
4Protection against splashesSplashing water from any direction
5Protection against water jetsLow-pressure jets, limited ingress permitted
6Protection against strong jetsHigh-pressure jets, limited ingress permitted
7Protection against immersionTemporary immersion (up to 1m depth, 30 mins)
8Protection against prolonged immersionContinuous immersion beyond 1m
9KProtection against high-pressure hot water jetsHot, high-pressure water jets (food industry/washdowns)

 

Water ingress protection is vital since moisture can cause corrosion, short circuits, and ignition sources in explosive atmospheres.3 

How IP Ratings Impact Safety in Hazardous Environments

Ensuring Protection Against Dust and Particles

Dust, especially combustible dust, can accumulate inside enclosures, leading to increased fire and explosion risks. Dust-tight enclosures (IP6X) are critical to prevent dust ingress that could interfere with electrical operation or become an ignition source.

Water Resistance and Its Importance in Explosive Atmospheres

Ingress of water, whether from rain, splashing, jets, or immersion, can cause short circuits, corrosion, and other failure modes that may ignite explosive gases or dust. Higher liquid protection levels ensure safety and operational integrity in exposed industrial settings.

Compliance with Safety Standards

IP ratings complement explosion protection standards such as EN and IEC by fortifying the enclosure’s ability to resist environmental elements that might compromise explosion safety. Proper IP-rated sealing preserves the enclosure’s flameproof function and meets regulatory requirements.3 

How to Choose the Right IP Rating for Your Ex Enclosure

Assessing Environmental Factors and Hazards

Consider the hazardous zone classification, presence of dust or vapors, climate conditions (e.g., humidity, rainfall), and exposure to washdowns or submersion.

Matching the IP Rating to the Location and Equipment

  • For dusty, dry environments: aim for IP6X (dust-tight) at minimum.
  • For wet, outdoor, or washdown environments: consider IP65, IP66, or higher.
  • For exposure to immersion: IP67 or IP68 may be needed.
  • For food or pharmaceutical industries requiring hot washdowns: IP69K offers protection against high-pressure hot water jets. 

Material and Volume Considerations

Choose materials like stainless steel for harsh environments, and ensure sufficient internal volume to avoid pressure piling, temperature rise and hot surfaces in Ex enclosures. Consult manufacturer data sheets for exact protection limits.

The Role of IP Ratings in Enclosures for Industrial Safety

Stainless Steel Enclosures and Their Resistance to Harsh Environments

Stainless steel’s corrosion resistance makes it ideal for maintaining high IP ratings in marine, chemical, refineries and food production environments where hygiene or hazardous atmospheres  and durability under washdowns are priorities.2 

Compact Enclosures with High IP Ratings for Small Spaces

Rittal offers compact enclosures with high IP ratings to deliver space-efficient, durable protection for industrial applications needing reliable ingress resistance in constrained areas.2 

The Importance of IP Ratings for Control Panel

Protection of Electrical Components in Harsh Conditions

Control panels house critical devices vulnerable to dust and moisture. The correct IP rating prevents ingress that could lead to failure, fires, or unsafe conditions.

How to Maintain Optimal Safety in Control Panels with the Right IP Rating

Ensure proper sealing of cable glands and panel interfaces. Regular maintenance to inspect and replace seals preserves ingress protection and explosion safety.

Common Mistakes to Avoid When Choosing IP Ratings for Ex Enclosures

  • Assuming higher IP digits always imply cumulative protection without verifying specific conditions (e.g., IPX7 ≠ IPX6).
  • Misinterpreting the meaning of IP ratings related to underwater use or chemical resistance.
  • Overlooking the importance of adequate internal volume to avoid pressure piling in Ex d enclosures.
  • Neglecting regular maintenance of seals and gaskets.
  • Relying solely on IP rating without considering full explosion protection certification.

FAQs

It defines the degree of protection against ingress of solids and liquids, crucial for maintaining explosion and fire safety.

Assess environmental exposure, hazard classification, and operational requirements with manufacturer guidance.

India's varying climate and industrial conditions require protection against dust, monsoon rains, and washdowns.

Yes, especially when combined with appropriate gasket materials like silicon and enclosure material stainless steel that withstand harsh conditions.