Liquid Cooling Packages
-
Liquid Cooling Package LCP Rack DX
Closed loop in row direct expansion cooling unit efficiently maintains proper server inlet temperatures contained entirely within the rack system.
-
Liquid Cooling Package LCP Inline DX, UL
Open loop in row direct expansion cooling unit efficiently maintains proper server inlet temperatures.
-
Liquid Cooling Packages LCP Rack CW
For the highest density installations, these LCP Rack units totally control the air path for efficient cooling. The LCP Rack CW is a closed loop system and units are scalable from as low as 10kW to as high as 60kW with all the most requested stops in between. These new, more powerful units in the line maintain the 12-inch wide footprint – making it possible, in some situations, to double the cooling capacity without taking up additional floor space.The unit’s high-efficiency fans have been moved to the front of the LCP – on the cool side away from maximum heat – which will extend the life of the fans. Water connections are available at either the top or bottom of the unit.
-
Liquid Cooling Package LCP Inline CW
These highly efficient Inline units can create a cold curtain down a row rather than simply moving air into an aisle.Available in two versions: Flush, a configuration where the unit’s face matches that of the adjacent enclosures and air flows into the racks; and Protruding where the unit is bumped out 8 inches into the aisle and cool air flows from both sides across the face of nearby enclosures.The unit’s high-efficiency fans have been moved to the front of the LCP – on the cool side away from maximum heat – which will extend the life of the fans. Water connections are available at either the top or bottom of the unit.