Sizing enclosure climate control by hand is slow, and easy to get wrong. Undersize it and components overheat. Oversize it and you waste energy and budget on cooling you didn't need. RiTherm, Rittal's free planning tool, is built to remove that guesswork.
Why Manual Thermal Calculations Fall Short
Getting enclosure cooling right means accounting for internal heat load, ambient temperature, altitude, enclosure material and airflow, all at once. Doing that manually, project after project, invites two failure modes: an undersized system that shortens component life through heat stress, or an oversized one that adds cost and energy use without a real benefit. Rittal has offered a free calculation tool for this exact problem for 35 years, evolving it into RiTherm, now used for more than 200,000 climate control calculations a year.
What RiTherm Actually Calculates
RiTherm handles both indoor and outdoor installations, and lets the user specify site altitude, since air density at altitude directly affects cooling output. For bayed enclosure suites, it supports custom "heat loss zones", letting different sections of a large assembly be modelled as one interconnected thermal area rather than forcing a single uniform calculation across the whole suite. The result is a specific, documented recommendation for the right cooling unit, fan-and-filter unit or heat exchanger, not a generic rule of thumb.
Built for Compliance, Not Just Cooling
Beyond sizing, RiTherm generates the paperwork a project actually needs. It produces a standards-compliant heat dissipation certificate, relevant under the EU's Machinery Regulation framework, along with a bill of materials and product lifecycle information, including notice when a component has a successor part. For refrigerant selection, RiTherm surfaces GWP data directly in the design process, which matters given the F-Gas Regulation's tightening limits on refrigerants used in enclosure cooling. The tool also calculates the carbon footprint of the proposed climate control solution, from delivery through to operation, which more end customers are now asking their panel builders and integrators to document, even where it isn't yet a legal requirement.
Built for Real Projects, Not Just Single Enclosures
RiTherm works whether the project is a single enclosure, a full bayed suite, an outdoor installation, or even equipment that isn't Rittal's own. It integrates with Eplan Cloud, so project data can move between design tools instead of being re-entered, and documentation can be exported as PDF, DOCX, XML or HTML depending on what the project needs. Teams can also collaborate on the same project within their organisation rather than each engineer working from a separate file.
Why This Matters for Greek Panel Builders
For panel builders and system integrators in Greece, RiTherm's real value is in the paper trail as much as the calculation. As the EU's Machinery Regulation phases in and end customers increasingly ask for documented energy-efficiency and carbon-footprint evidence, having that documentation generated automatically at the design stage, rather than reconstructed after the fact, saves time on every project and reduces the risk of a compliance gap being found late.
FAQ
What is RiTherm?
RiTherm is Rittal's free planning software for calculating the climate control requirements of enclosures, covering both indoor and outdoor installations, with standards-compliant documentation generated automatically.
Is RiTherm free to use?
Yes, Rittal has offered its thermal calculation software as a free tool for 35 years, and RiTherm is the current version, used for more than 200,000 calculations a year.
Does RiTherm work for outdoor enclosures?
Yes, RiTherm calculates climate control requirements for both indoor and outdoor installations, accounting for ambient conditions and site altitude.
Can RiTherm calculate cooling for a full suite of bayed enclosures, not just one cabinet?
Yes, RiTherm supports custom heat loss zones, allowing sections of a bayed enclosure suite to be modelled as a single connected thermal area.
Does RiTherm help with F-Gas Regulation compliance?
Yes, RiTherm surfaces GWP data for refrigerant options during the design process, helping panel builders choose compliant refrigerants as F-Gas Regulation limits tighten.
What documentation does RiTherm generate?
RiTherm produces a standards-compliant heat dissipation certificate, a bill of materials, and product lifecycle information, exportable as PDF, DOCX, XML or HTML.
Does RiTherm only work with Rittal enclosures?
No, RiTherm can calculate climate control requirements for enclosures from other manufacturers as well as Rittal's own range.
How does RiTherm calculate carbon footprint?
RiTherm calculates the carbon footprint of the proposed climate control solution across its full lifecycle, from delivery through to operation, which end customers increasingly ask panel builders to document.