C rails

  • C rails 30/15 to EN 60 715 for VX, TS, SE
    C rails 30/15 to EN 60 715 for VX, TS, SE

    For direct installation on the horizontal enclosure section, on the base configuration rail for CM, on the vertical enclosure section via additional assembly components.

    More

  • C rails for TS, SE
    C rails for TS, SE

    For direct external mounting between the vertical TS, SE enclosure sections. The C-section angle bracket is additionally required for mounting between the horizontal TS, SE enclosure sections. Thanks to the universal attachment piece, the C rails may be optionally attached to the inner or outer level of the TS 8 frame.

    More

+
[X] Close

Required