Finance

Digitalization – fresh opportunities for the financial sector

Technologies such as blockchain and cryptocurrencies are throwing up new challenges for the financial sector. Above all, however, they offer fresh opportunities and possibilities for improving efficiency and security. Rittal provides the perfect solutions to meet financial institutions’ data management and data security requirements.

Innovative technologies and forms of mobile communication that are creating new structures and processes by capturing, transferring and evaluating large volumes of data are opening up big opportunities for financial institutions to expand the range products and services they offer. Thanks to online banking, customers can do their banking anywhere and at any time. And when it comes to corporate customers, the digitalization of the financial sector is creating new options and areas of business. Banks are gaining new insights into what their corporate customers do with the money they have received from them. Depending on the individual case, this may help assess the risk of a transaction, for example. In other words, banks are far more directly involved in processes.

Availability and security are top priorities

The new technical possibilities are improving the availability of services. Customers expect to be able to bank using various channels, selecting their preferred method and switching whenever they wish. This omnichannel approach aims to network all channels so as to ensure easy switching at any time, also maintaining or even improving customer satisfaction through end-to-end availability. The digital challenge means omnichannel availability has become one of the most important strategies in the financial sector.

One trend that will change the sector for ever is blockchain. This new disruptive technology makes it possible to keep a global register that unambiguously assigns ownership and helps transfer assets in seconds if necessary. In the case of payments, for example, blockchain technology enables fully anonymous transactions between users without a central financial intermediary. All the parties involved check and document each transaction, which prevents subsequent tampering. Although cryptocurrencies such as Bitcoin have raised the profile of blockchain technology in recent years, it also offers considerable potential and a whole host of opportunities in many other sectors of the economy. For example, blockchain can be used in electronic trading systems such as after-hours trading. Blockchain technology has been taken to the next level with smart contracts. In this case, the blocks are not restricted to simple financial transactions but include entire contracts relating to securities such as shares, bonds, futures and loans.

To get the most out of these new options, banks and financial institutions require a fail-safe, state-of-the-art infrastructure that ensures high availability and optimum cybersecurity. This is vital, because as the potential for the financial sector grows, so does the scope for hackers. Cutting-edge IT security should meet the challenges of digital transformation while also creating a solid foundation for further development.

Universal-Investment: Data centre installed in record time

To meet new market requirements and reflect the asset management company’s dynamic growth, Universal-Investment created a new data centre at its site in Frankfurt in collaboration with project partner Canzler Ingenieure. The RiMatrix S from Rittal was selected for the modular data centre, which is a security room in itself, complete with a physical access control system. It also incorporates a protective shell that affords further protection against fire, water and smoke. In the event of a power outage, the UPS unit installed in RiMatrix S steps in first, before the in-house diesel generator starts to supply backup power to the entire building.

Digitalization

Digitalization is creating new business models

Connected and smart, digitalization is having an impact in all sectors of industry.

IT 基础设施

数据中心解决方案

模块化集装箱数据中心提供完美的可扩展解决方案——无论是中型、云端和边缘应用,还是预先配置的集装箱式数据中心,都可以使用我们的模块化集装箱系统,您始终可为您的应用找到合适的解决方案。