Rittal strives to continuously improve its products; of course with input from the market. As part of this process, our new fan was created: The Rittal Blue e+ . The new generation of fans are available now. We would like to draw your attention to the fact that the new fans will replace the current TopTherm ones and the TopTherm range will be discontinued with effect from 30th April 2025.
Our new fan has been created with all the features and benefits of the current one, but also contains new innovations such as:
- Emergency cooling function for unexpected heat in the cabinet (EC fans)
- Higher air permeability by using a pleated filter mat
- Connection option for an IoT interface for information on status, usage, operating hours or energy consumption
- Automatic filter cleaning (only possible in combination with an IoT interface)
To enable a smooth transition, we have put together a corresponding conversion guide below.
View the corresponding notification letter here