AI Is Driving Data Center Energy Demand. Is the Infrastructure Ready?

December 07 2026

Author: Dimitris Tzerefos

Industry research now puts Europe's AI-driven electricity demand anywhere between 45 and 145 TWh by 2030, depending on how infrastructure and regulation evolve. Whichever path plays out, one thing doesn't change: the physical infrastructure behind it has to be ready.

Four Scenarios, One Certainty

A recent industry study modelled four distinct pathways for European AI electricity demand through 2030: a constrained scenario reaching around 45 TWh, a coordinated growth path around 90 TWh, an unregulated expansion scenario as high as 145 TWh, and a volatile path that oscillates between crisis and recovery. Globally, the picture points the same direction. The International Energy Agency projects data center electricity consumption will roughly double by 2030, with AI-specific demand growing even faster than the overall total.

The exact number that materialises depends on regulation and grid investment. What doesn't depend on any of that is the direction: demand is going up, and facilities need infrastructure built to absorb it, not retrofitted after the fact.

Cooling: Built for the Full Range, From Edge Rack to Hyperscale

Air cooling runs out of headroom well before AI racks do. Rittal's Direct Liquid Cooling (DLC) portfolio covers that gap across three tiers rather than a single fixed solution: liquid-to-air systems that cool the chip directly and reject heat via the rack's rear door, suited to individual racks or moderate heat loads; and liquid-to-liquid systems, cooled by the building's own water supply, built for bayed, high-performance and hyperscale deployments delivering up to 1 MW of cooling output. For rack-level deployments not needing a full liquid loop, the LCP Rear Door CW dissipates up to 53 kW per rack via an air/water heat exchanger, with intelligent fan control capable of cutting energy use by up to 50% at partial load.

What differentiates the range operationally is serviceability: hot-swap components let critical parts, pumps, sensors, controllers, be replaced while the system keeps running, and integral N+1 redundancy means a single component failure doesn't take the rack offline. For a facility scaling toward any of the higher-demand scenarios, that combination, output headroom plus zero-downtime maintenance, is what makes a density upgrade a planned step rather than a disruptive rebuild.

Power Distribution: Scaling Without Starting Over

Cooling gets most of the attention, but power distribution capacity decides the ceiling just as often. RiLineX handles the lower end with a tool-free, 60 mm busbar platform rated up to 800 A, click-in assembly, and IEC 61439 and UL 508A approvals, so lower-density racks and edge deployments aren't over-engineered with switchgear sized for hyperscale loads. For larger assemblies, Ri4Power builds on the VX25 enclosure platform, scaling up to 6300 A and supporting circuit-breakers from major manufacturers, tested as a complete IEC 61439-compliant system rather than assembled piecemeal on site. Between the two, a facility can size power distribution to its actual load today and add capacity in stages as demand grows, instead of over-building from day one or rebuilding once density arrives.

Edge Deployments: The Same Standards, a Smaller Footprint

Not every facility is a hyperscale build. RiMatrix Micro Data Center packages enclosure, cooling, power and monitoring into a single pre-configured, self-contained unit for edge and distributed IT sites, bringing the same design principles behind Rittal's larger data center portfolio to locations that don't need, or can't host, a full facility build-out.

Why This Matters for Greek Data Centers and Colocation Providers

Greece's colocation and data center sector is growing from a smaller base than Western Europe's established hubs, which is an advantage here: new capacity can be specified with DLC-ready cooling and modular power distribution from day one, rather than retrofitted onto infrastructure built for lower-density loads. For panel builders and system integrators serving this market, that means the Rittal product tier chosen now, RiLineX-level, Ri4Power-scale, or full DLC, should match where load is heading, not just where it sits today.

FAQ

How much could AI increase Europe's electricity demand by 2030? 
Industry modelling puts the range between roughly 45 TWh under constrained growth and 145 TWh under unregulated expansion, with a coordinated growth path around 90 TWh.

Is this only a European issue? 
No. The International Energy Agency projects global data center electricity consumption will roughly double by 2030, with AI-specific demand growing faster than the overall total.

What cooling output does Rittal's Direct Liquid Cooling portfolio support? 
Rittal's DLC range spans individual-rack liquid-to-air systems up to bayed liquid-to-liquid solutions delivering up to 1 MW of cooling output for hyperscale deployments.

Can Rittal's cooling systems be serviced without shutting the rack down? 
Yes. DLC and LCP systems support hot-swap replacement of components like pumps and controllers, with N+1 redundancy so a single failure doesn't interrupt operation.

What's the difference between RiLineX and Ri4Power for data center power distribution? 
RiLineX is a tool-free 60 mm busbar platform rated up to 800 A, suited to lower-density and edge deployments. Ri4Power builds on the VX25 enclosure for larger assemblies, scaling up to 6300 A.

Is there a Rittal solution for smaller or edge data center sites? 
Yes. RiMatrix Micro Data Center packages enclosure, cooling, power and monitoring into a single pre-configured unit for edge and distributed IT locations.

Should Greek data centers plan differently because the market is newer? 
In some ways, yes. Newer facilities can specify DLC-ready cooling and modular power distribution from the start, rather than retrofitting infrastructure built for lower loads.

What should panel builders take away from this uncertainty? 
Match the product tier to where load is heading, not where it sits today. Underbuilding capacity tends to cost more later than building in headroom now.