Integrated RiMatrix HPC architecture brings together direct liquid cooling, standardized racks and an 800 VDC Power Sidecar concept to address the demands of next-generation computing.
CHICAGO, Ill., November 15-20, 2026 — As artificial intelligence and high-performance computing (HPC) push data center power densities to new levels, Rittal will showcase an integrated infrastructure approach designed to help operators scale computing capacity while addressing growing challenges in power distribution, thermal management and system deployment at SC26, the international conference for high-performance computing, networking, storage and analysis, at McCormick Place in Chicago, Illinois.
Building on its presentation at the 2026 Open Compute Project (OCP) Global Summit, Rittal will demonstrate how its RiMatrix HPC architecture brings together standardized high-performance racks, direct liquid cooling and DC power infrastructure in a compact, modular system designed for increasingly demanding AI and HPC environments.
The approach addresses three interconnected infrastructure priorities: creating a scalable foundation for high-density computing, managing growing thermal loads and delivering the power required to support next-generation systems.
A system approach to high-density computing
By integrating rack infrastructure, cooling and power distribution into a coordinated system, Rittal's RiMatrix HPC architecture is designed to simplify infrastructure planning and deployment, improve operational efficiency and support scalable growth as computing demands increase.
The architecture brings together three essential technologies, each addressing a critical requirement of high-density AI and HPC environments:
- Standardized high-performance racks: Provide a modular, repeatable foundation that supports high-density computing hardware, simplifies infrastructure planning and enables future expansion.
- Direct liquid cooling: Rittal's Coolant Distribution Unit (CDU) technology delivers more than one megawatt of water-based cooling capacity for direct-to-chip applications, with modular units designed to support maintenance during operation.
- Integrated DC power distribution: An 800 VDC Power Sidecar development concept incorporating power electronics from Bosch and Rittal's RiLineX busbar platform is designed to support scalable, high-density power infrastructure aligned with emerging OCP architectures.
Scalable infrastructure: Building a foundation for high-density computing
As computing requirements grow, data center operators need infrastructure that can expand without requiring every deployment to be engineered from the ground up.
Rittal's RiMatrix HPC architecture addresses this challenge through standardized, modular infrastructure designed to integrate high-performance racks, cooling and power distribution into a coordinated system.
Based on open OCP architectures, the approach supports repeatable infrastructure configurations that can help simplify planning, deployment and future expansion.
Rather than treating racks, power and cooling as independent components, Rittal's system approach brings these technologies together to support increasingly concentrated computing environments.
Advanced cooling: Managing the thermal demands of AI and HPC
As processors and accelerators generate greater heat loads, traditional air-based cooling approaches face increasing limitations. Higher computing densities require cooling infrastructure that can manage thermal loads efficiently while supporting system availability and serviceability.
Rittal's Direct Liquid Cooling portfolio is designed to address these requirements by bringing cooling closer to the heat source.
The portfolio includes modular Coolant Distribution Unit (CDU) technology for direct-to-chip applications, including high-capacity solutions designed for megawatt-scale cooling requirements.
Rittal's CDU technology incorporates modular components designed to support maintenance during operation, helping operators manage service requirements while maintaining cooling availability.
Integrated into the broader RiMatrix HPC architecture, the cooling system supports a coordinated approach to infrastructure planning, allowing thermal management to evolve alongside computing capacity.
Integrated power distribution: Preparing for the next generation of computing
Managing higher thermal loads is only part of the challenge. As AI and HPC systems demand greater computing performance, power infrastructure must also evolve to support higher densities and increasingly compact deployments.
At SC26, Rittal will highlight its 800 VDC Power Sidecar development demonstrator, featuring high-power-density power electronics from Bosch.
The technology draws on Bosch's experience with 800-volt systems in electric vehicles, with power electronics being further developed for continuous operation in data center environments.
The modular concept is designed to support scalable power supply solutions of up to 2 MW. Rittal integrates this technology with its RiLineX busbar platform into a sidecar architecture oriented toward OCP standards.
The demonstrator illustrates how emerging DC power architectures could support higher power transmission and more compact infrastructure as AI and HPC requirements continue to evolve.
Bringing the infrastructure together
The value of Rittal's approach lies in the integration of these three infrastructure elements.
By combining standardized rack architecture, direct liquid cooling and power distribution into a coordinated system, RiMatrix HPC is designed to provide a repeatable foundation for increasingly demanding computing environments.
As a long-standing member of the Open Compute Project, Rittal continues to apply its experience in standardized infrastructure and system integration to the development of open computing architectures.
For hyperscale operators, HPC facilities, system integrators and data center infrastructure teams, the approach offers a framework for evaluating how cooling, power and rack technologies can work together to support future computing requirements.
Visit Rittal at SC26
Attendees can learn more about Rittal's integrated infrastructure approach at Booth #4234 November 15-20 at McCormick Place in Chicago, Illinois.
For more information about Rittal's solutions for high-performance computing, visit Rittal at SC26.
Media Contact
Krista Topacio
Public Relations and Paid Media Marketing Manager
Rittal LLC
topacio.k@rittal.us
About the Event
Event: Super Compute 2026
Date: November 15-20, 2026
Location: McCormick Place Chicago, IL 60616
More Information: One Vendor. One Ecosystem. Trusted for the Future
About Rittal LLC
Founded in 1982, Rittal LLC is the fully owned US subsidiary of Rittal GmbH & Co. KG, and is headquartered in Schaumburg, IL. With a main production facility in Urbana, OH, a dedicated Modification Center in Houston, TX, and logistic hubs in Urbana, OH; Springfield, OH; Houston, TX; Sparks, NV; and Atlanta, GA, Rittal LLC is fully committed to providing the United States with quality enclosure solutions.
Founded in 1961 in Germany, Rittal is a global manufacturer of industrial and IT enclosures, racks, and accessories, including cooling solutions and power management systems for industrial, data center, outdoor, and hybrid applications. As the largest enclosure manufacturer in the world, Rittal provides quality solutions for practically any industrial or IT infrastructure application. Rittal is part of the owner-operated Friedhelm Loh Group along with Eplan.