Viega GmbH

"... the MDCs Level E have everything we need.”

In need of a new data centre, but short on both space and time, Viega in Attendorn found a quick and practical solution. Two Rittal Micro Data Centers Level E provided this leading supplier of installation technology for sanitary facilities and heating systems with the necessary redundancy, while also ensuring all new safety and security standards were met.

Overview

Project
Viega GmbH
Location
Attendorn, Germany
Challenge

Lack of redundancy with former IT infrastructure

Lack of space

No possibility for structural modifications

Quick solution required; no time frame for new construction

Need for modern fire protection and safety standards

Growing IT systems as the company expands

Goal: CO₂-neutral production by 2035 at the latest

Elimination of environmentally harmful coolants

IT systems must be protected and have controlled access

Solution

Use of two immediately available Micro Data Centers MDC Level E

Distribution across two locations / fire compartments within the building

Compact design requiring no additional new construction

Protection against: Dust, dirt, smoke, fire, mechanical impacts

Automatic gas extinguishing system

Integration into Viega’s internal monitoring system

Installation in separate rooms for controlled access management

Environmentally friendly cooling without problematic refrigerants

Fast delivery and careful implementation by Rittal

Modularly expandable and scalable for further growth

 

MDCs Level E, on the other hand, are both streamlined and reliable. They have everything we need, with no unnecessary frills.
Leon Wurm, Viega

Global market leaders need world-class IT infrastructure. “Before we got the Rittal Micro Data Center Level E, some parts of our IT infrastructure, which had grown organically, lacked redundancy,” reports Leon Wurm, Network Administrator at Viega. What’s more, the available space offered no scope for the structural changes that would have been necessary, for example, to extend the expanding company’s IT systems and implement up-to-date fire safety measures. 

The IT specialists and the facility management team were looking for a quick and practical solution. They wanted to split the IT infrastructure between two locations in different fire compartments in the building and provide urgently needed redundancy without taking up too much space. There wasn’t time to build a new data centre with a separate security room. 

Micro Data Center Level E for maximum performance 

The company ultimately opted for two Rittal Micro Data Centers (MDCs) Level E, each with four bayed enclosures, on different floors of the building – with sufficient capacity to map all production-related applications and also ensure the necessary redundancy. The clock was ticking for Rittal. The solution needed to be ready as soon as humanly possible, without compromising on security or fire safety.

Fortunately, MDCs Level E meet the relevant requirements as standard. The rack technology’s level of protection against dust, dirt, smoke, fire, impacts, etc. means no further physical protective measures are necessary. For safety reasons, Viega nonetheless installed the MDCs Level E in separate rooms rather than in the actual production area. “That was a request and a requirement from our IT team – amongst other things, to ensure access could be controlled,” Wurm explains.

The MDCs’ Level E fire safety monitoring was incorporated directly into Viega’s in-house monitoring system. If an alarm is triggered, nobody even needs to call the fire service, because the integrated gas extinguisher system automatically reduces the amount of oxygen in the air enough to suppress any spark. Once the gas extinguisher has done its job, the doors can simply be opened again. This is preferable to sprinkler systems, which can quickly damage the sensitive electronics.

Further key factors in Viega’s decision included its appreciation of how quickly but conscientiously Rittal works, the MDCs’ Level E high-quality workmanship, and integrated services such as power supply and water cooling. “By 2035 at the latest, we want Viega to have completely carbon-zero production operations, so there was no question of us using a potentially environmentally harmful refrigerant,” says Wurm. 

Guaranteed future-proofing

Meeting the requirements perfectly wasn’t the only impressive thing about the solution. “The MDC Level E will ensure we remain incredibly flexible in the future,” Wurm emphasises. After all, the system can be extended at any time. What started at the headquarters in Attendorn is now well on the way to becoming the new standard at the company. Viega has already ordered two further Rittal MDCs Level E for the company’s Grossheringen site in Thuringia, its largest production site anywhere in the world. Another site, which is currently being built in Kirkel, in the Saarland region, is also set to be equipped with this system. “Many data centres from other manufacturers often require large investments and come with numerous features we don’t need. MDCs Level E, on the other hand, are both streamlined and reliable. They have everything we need, with no unnecessary frills,” Wurm concludes.