ELECTRIFY YOUR SYSTEM

Charging infrastructure, energy efficiency and sector coupling

Take the right path to energy transition with strong partners

Energy Consumption

Solutions for energy consumption

Energy transition does not end with the distribution and storage of electricity. Energy consumption also plays a major role and has several different considerations. For example, it is about efficient energy management, with which businesses, especially the manufacturing industry, can reduce power consumption. Sector coupling, or in other words connecting the electricity, heating, building, transport and other industrial sectors, is another important component of energy transition.

With regard to increasing e-mobility, it is crucial to make electricity available at many decentralized points: in charging parks, at home, at work or when shopping. In short, charging infrastructure is needed wherever the car is parked.

Innovative concepts with in the FLG group 

Integrated hardware and software solutions are increasing the pace of energy transition. Rittal is tackling these new issues together with its sister companies Eplan and GEC so it can digitalize and automate processes. In this way, it will be possible for even complex systems and tasks to be mapped with greater clarity and prepared for the future more quickly.

The most effective results are from best-practice examples based on many customer projects that have been undertaken. For example, there are pre-designed solutions for the planning and implementation of charging parks that the planner can easily access in electrical engineering with Eplan. The pre-configured project contains every detail, including standardized industrial hardware, and only calls for minimal customisation – time saving par excellence.

Your benefits at a glance:

  • Planning and implementation in record time – best-practice solutions exist and are available instead of elaborate new designs
  • First-class quality – error-free project planning with tried and tested solutions
  • Perfect synergy and co-ordination – hardware and software are perfectly matched to each other
  • Global application options through compliance with international standards and worldwide service
  • Forward-looking partners with new and innovative solutions for energy transition – for the competitiveness of your company

Typical solutions for charging infrastructure:

Outdoor

CS Toptec

Outdoor enclosure with 100 mm transport base/plinth and rain canopy with projections on all sides. Side panels, rear panel and door fully double-walled on the outside, the entire TS8 frame is available for interior installation.

Enclosures

Wall-Mounted Enclosures

Wall-mount enclosure and case solutions in the following versions: carbon steel, stainless steel, and fiberglass reinforced polyester. Extremely versatile for control applications with moderate space requirements. Fulfill the most stringent corrosion...

Enclosures

Outdoor

Outdoor enclosures are ideal for use outside. Rittal’s CS wall-mounted enclosures and CS New Basic enclosures are available off the shelf as standard products. CS Toptec enclosures are the perfect solution for all your outdoor projects. The...

Power Distribution

Busbar Systems

RiLine busbar systems for individual switchgear and controlgear up to 2100 A. Complete solutions for AC or DC applications.

Success Stories.

Tritium

E-mobility for everybody

The international availability and quality of Rittal products were decisive factors in winning the order from Tritium. The Rittal solution is also used, among other things, to protect the sensitive electrical components of the charging stations from...

SBRS GmbH

Protected from rain and sunshine

The German city of Freiburg boasts a fleet of climate-friendly electric buses. These buses benefit from an ingenious charging infrastructure from SBRS GmbH incorporating Rittal components that offer ideal protection against the elements and unauthorised...

Gemamex

Sofia – electric buses rapidly charged thanks to the VX25

Thirty electric buses are in service in the Bulgarian capital of Sofia. The charging infrastructure consists of Rittal VX25 enclosures, specially assembled into a three-unit combination for Gemamex, the manufacturer of the fast-charging stations.

Kölner Verkehrs-Betriebe/SBRS GmbH

Charged up in 60 minutes

Charging infrastructure is one of the major stumbling blocks as we switch to electric mobility. For example, if urban bus routes are changed to e-mobility, they will also need powerful charging stations. The Cologne Public Transport Authority (Kölner...