3311410 - LCP Rack DX, 300x2000x1000

  • The LCP draws in the air at the sides at the rear of the server enclosures, cools it using high-performance compact impellers, and blows the cooled air back into the front part of the server enclosure at the sides
  • Maximum energy efficiency thanks to EC fan technology and IT-based control
  • Thanks to the speed-regulated compressor, the cooling output is ideally adapted to actual requirements
  • Ideal for IT cooling of small and medium-sized locations
  • One or two racks can be cooled separately
Picture shows similar models
Add accessories?
General
SNMP card
Also required
Condenser unit
Add to enquiry list