Wishlist

RiDiag

Diagnosis and analysis for cooling units

RiDiag is a diagnosis and analysis program which serves to monitor the proper functioning of cooling units and, in doing so, to simplify maintenance and the interpretation of system messages.

RiDiag can be used in the following versions:

NEW RiDiag III: For analysis and extended parameterisation of all Rittal cooling units and chillers of the Blue e+ series: With RiDiag III, all relevant parameters and settings can be entered for the units, and all system messages are displayed in plain language with corresponding help texts. Service and spare parts enquiries can be submitted directly from within the software. RiDiag III also permits the retrospective analysis of all saved units and component data for up to two years (add-on function). The connection to the units is made via a USB to micro-USB cable (not included in the scope of supply).

RiDiag II: Parameterisation and extended settings for all Rittal cooling units of the Comfort and Blue e series: With RiDiag II, parameters and extended settings can be entered for the units, and the error memory can be read out. Long-term data from the units can be logged and analysed. The connection to the units is made via a special cable which is included in the scope of supply of 3159.100.

RiDiag I: Parameterisation and diagnosis for all Rittal cooling units with microcontroller. With RiDiag I, parameters can be entered for the units and the error memory can be read out. The connection to the units is made via a special cable which is included in the scope of supply of 3159.000.

Further information

Model No.: SK 3159.100 (RiDiag 2)

  • RiDiag III
    Model no.: SK 3159.300 (for enabling of add-on functions by way of a paid licence)
    Download
  • RiDiag II Version 3.4 (8.68 MB)
    Model no.: SK 3159.100
    Download
  • RiDiag I (3.36 MB)
    Download

For technical queries, please use one of the worldwide Rittal contacts